Skip to main content
Graduate
May 14, 2025
Solved

STEVAL-SMARTAG2 problems with creating new project

  • May 14, 2025
  • 1 reply
  • 276 views

Hello, I'm using STEVAL-SMARTAG2. In the future I want to design my own PCB with  ST25DV64KC and STM32L4P5-CGU6. But for now I want to create my own program and try it on STEVAL-SMARTAG2.

If I import example project in CubeIDE and complie it, It works fine.

If I want to create my own project and include libraries I get an errors during compiling.

So, I did the following:

- start new project in CubeIDE and select "STEVAL-SMARTAG2"

- set inputs/outputs as default (press OK when pop-up window ask me if i want to keep it)

- middleware/software package... download and select FP-SN-SMARTTAG2

- define platform settings (picture below)

image.png

- save and run the compiler and get an errors (picture below)

image.png

It looks like I miss something?

Also in my further project I don't need to use all the sensors on the protoboard. I just want to use NFC-V and powering tag with energy harvesting.

 

Thank you for your time.

 

 

    This topic has been closed for replies.
    Best answer by Berenice BENVEGUDA

    Hello,

     

    First of thanks for your interest in ST25 products !

    Then, the details described are not sufficient to well identify the problem.

    The file SmarTag_test1.ioc (STM32CubeMX configuration file for the generated project ) will be necessary.

    What can be said is that:

    • In the first picture  "Board Support STEVAL-SMARTAG2" is in yellow color.
    • This means that a few components have not been included in the "Select Components" phase: I suppose NFC7 board extension and X-CUBE-MEMS1 driver components.

    I hope this helps,

    Best Regards,

    BB

    1 reply

    Technical Moderator
    May 22, 2025

    Hello,

     

    First of thanks for your interest in ST25 products !

    Then, the details described are not sufficient to well identify the problem.

    The file SmarTag_test1.ioc (STM32CubeMX configuration file for the generated project ) will be necessary.

    What can be said is that:

    • In the first picture  "Board Support STEVAL-SMARTAG2" is in yellow color.
    • This means that a few components have not been included in the "Select Components" phase: I suppose NFC7 board extension and X-CUBE-MEMS1 driver components.

    I hope this helps,

    Best Regards,

    BB