STM32F407VG + M24SR
I'm trying to connect m24sr to stm32f407vgt.
I switch to I2C2, clocking from an external resonator at 8 MHz, SYSCLK 72 MHz, I use a converted library for Open107V. For stm32f107vc this code worked, but when switching to stm32f407 i2c does not work (most likely there is no response from m24sr and a timeout error occurs).I've been puzzling for several days, I can not find the error.
Defines for i2c
&sharpdefine M24SR_SDA_PIN GPIO_Pin_11
&sharpdefine M24SR_SDA_PIN_SOURCE GPIO_PinSource11&sharpdefine M24SR_SDA_PIN_PORT GPIOB&sharpdefine M24SR_SCL_PIN GPIO_Pin_10
&sharpdefine M24SR_SCL_PIN_SOURCE GPIO_PinSource10&sharpdefine M24SR_SCL_PIN_PORT GPIOB&sharpdefine M24SR_GPO_PIN GPIO_Pin_15
&sharpdefine M24SR_GPO_PIN_PORT GPIOD&sharpdefine M24SR_RFDIS_PIN GPIO_Pin_14
&sharpdefine M24SR_RFDIS_PIN_PORT GPIOD&sharpif defined STM32F40_41xxx
&sharpdefine M24SR_GPIO_BLOCK_CLK (RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOD)&sharpelse&sharpdefine M24SR_GPIO_BLOCK_CLK (RCC_APB2Periph_GPIOB | RCC_AHB1Periph_GPIOD)&sharpendif/ * I2C config ---------------------------------------------- -------------------------------- * /
&sharpdefine M24SR_I2C I2C2&sharpdefine M24SR_I2C_BLOCK_CLK RCC_APB1Periph_I2C2&sharpdefine M24SR_I2C_CLOCKSPEED 400,000The code itself
void M24SR_Init (void)
{M24SR_I2CInit ();M24SR_InitStructure ();
&sharpifdef I2C_GPO_SYNCHRO_ALLOWED
M24SR_KillSession ();M24SR_RFConfig (0);M24SR_ManageI2CGPO (I2C_ANSWER_READY);M24SR_Deselect (); &sharpendif / * I2C_GPO_SYNCHRO_ALLOWED * /}void M24SR_I2CInit (void){GPIO_InitTypeDef GPIO_InitStructure;I2C_InitTypeDef I2C_InitStructure;/ * GPIO Periph clock enable * /
&sharpif defined STM32F40_41xxxRCC_AHB1PeriphClockCmd (M24SR_GPIO_BLOCK_CLK, ENABLE);&sharpelseRCC_APB2PeriphClockCmd (RCC_APB2Periph_AFIO | M24SR_GPIO_BLOCK_CLK, ENABLE);&sharpendif/ * I2C Periph clock enable * /
RCC_APB1PeriphClockCmd (M24SR_I2C_BLOCK_CLK, ENABLE);/ * Configure I2C pins: SCL and SDA * /
GPIO_InitStructure.GPIO_Pin = M24SR_SCL_PIN | M24SR_SDA_PIN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;&sharpif defined STM32F40_41xxxGPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;&sharpelseGPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD;&sharpendif GPIO_Init (M24SR_SDA_PIN_PORT, & GPIO_InitStructure);&sharpif defined STM32F40_41xxx
/ * Connect I2C pins to AF * / GPIO_PinAFConfig (M24SR_SCL_PIN_PORT, M24SR_SCL_PIN_SOURCE, GPIO_AF_I2C2); GPIO_PinAFConfig (M24SR_SDA_PIN_PORT, M24SR_SDA_PIN_SOURCE, GPIO_AF_I2C2);&sharpendif/ * Configure GPIO for M24SR GPO as Input pull-up, used as Interuption comming from the M24SR * /
GPIO_InitStructure.GPIO_Pin = M24SR_GPO_PIN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;&sharpif defined STM32F40_41xxx GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;&sharpelseGPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;&sharpendif GPIO_Init (M24SR_GPO_PIN_PORT, & GPIO_InitStructure);/ * Configure GPIO for M24SR RF Disable signal * /
GPIO_InitStructure.GPIO_Pin = M24SR_RFDIS_PIN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;&sharpif defined STM32F40_41xxx GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;&sharpelseGPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;&sharpendif GPIO_Init (M24SR_RFDIS_PIN_PORT, & GPIO_InitStructure);I2C_DeInit (M24SR_I2C);
/ * I2C Init * /
I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = 0x00; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = M24SR_I2C_CLOCKSPEED; I2C_Init (M24SR_I2C, & I2C_InitStructure);/ * I2C Init * /
I2C_Cmd (M24SR_I2C, ENABLE);}
static void M24SR_InitStructure (void){/ * build the command * /Command.Header.CLA = 0x00;Command.Header.INS = 0x00;/ * copy the offset * /Command.Header.P1 = 0x00;Command.Header.P2 = 0x00;/ * copy the number of byte of the data field * /Command.Body.LC = 0x00;/ * copy the number of byte to read * /Command.Body.LE = 0x00;Command.Body.pData = DataBuffer;}uint16_t M24SR_KillSession (void){uint8_t pBuffer [] = {M24SR_KILLSESSION};int8_t status;errchk (M24SR_SendI2Ccommand (0x01, pBuffer));
/ * insure no access will be done just after open session * /
/ * The only way here is to poll I2C to know when M24SR is ready * // * GPO can not be used with KillSession command * /errchk (M24SR_PollI2C ());return M24SR_ACTION_COMPLETED;
Error:/ * Send STOP Condition * / I2C_GenerateSTOP (M24SR_I2C, ENABLE);return M24SR_ERROR_I2CTIMEOUT;}#stm32f407 #m24sr #i2c