Hello SStad.3,
which firmware is used to start-up the reader?
Is it ST firmware or a self developed version?
In any case - check the following:
- if the oscillator bit is not set then the PLL cannot lock either
- is a XTAL or a TCXO used?
- is the 20 MHz reference present?
- is the reader IC configured correctly for XTAL or TCXO - check register 0x0E.
if the 20 MHz reference is OK continue with the items below:
- automatic or manual VCO segment selected?
- refer to the VCO tuning range selection in the datasheet of ST25RU3993, section 2.3.1
- with the automatic VCO range selection the reader will select the best VCO segment.
- which frequency is set?
- check the PLL main register for value A and B
- check the correct settings of A and B according to the formula shown in the datasheet under 2.3.2.
- check the loop filter which is connected to pin LF_CEXT (pin 45)
- are the components correctly installed and do they have the correct values
When the reader is connected to a spectrum analyzer at which frequency is the reader output detected?
When it is purely a PLL locking issue then the carrier frequency will be instable.
I hope the items above are helping to solve the issue.
Cheers,
B