Skip to main content
Visitor II
October 30, 2019
Solved

Succesfull SendReceive write command to Mifare Ultralight EV1 sometimes responds with succes code, sometimes with error code

  • October 30, 2019
  • 1 reply
  • 923 views

Error - 8700 : Frame wait time out OR no tag

Even though a writeis succesfull, I will at one time get this error code back (this is the answer of the SendReceive, the result of SendReceive itself is errorcode '4 ' which stands for Communication Error), and another time a succes code. I know the write is succesfull because in the next read I can read the value that was written.

The problem with this is that I cannot check whether or not the write was succesfull and then try again, because this may put me in an infinite loop.

What can be the cause of this?

    This topic has been closed for replies.

    1 reply