T2T Emulation Response Failure
I'm working on emulating a T2T with my device. It successfully makes it through automatic anticollision, then starts looking for commands. When I see 0x30 0x00, I go ahead and send the first 16 bytes, but the reader does not react or show the read data.

Right now I'm thinking that I'm transmitting wrong while in Listen Mode. The RFAL never does T2T emulation, so I don't have an example there. Right now, when I see a 0x30 command, I do the following:
Send command CLEAR FIFO
Set Num Tx Bytes 1 to the MSB
Set Num Tx Bytes 2 mask 0xF8 to the LSB
Write the data to the FIFO
Send command TX WITH CRC
Is there a different way to do it in Listen Mode? With T2T Emulation the chip's field will never be on, but I don't see a way to explicitly modulate a response. The first 16 bytes are shown above, with the CC 0xE1 0x10 0x3F 0x0F. I do also have an empty NDEF TLV and the Terminator TLV, but no memory regions beyond the first 4 blocks are attempted to be read.
Also - I couldn't find any information on the INT2 byte after the second BCC, so I copied the 0x48 I've seen on NTAGs. What does that byte represent?