temperature sensor NDEF
I have programmed the temperature sensor, but it seems that it has not been successful, the NDEF reading result is shown in the figure, what should I do?
if( NfcType5_NDEFDetection( ) != NDEF_OK )
{
CCFileStruct.MagicNumber = NFCT5_MAGICNUMBER_E1_CCFILE;
CCFileStruct.Version = NFCT5_VERSION_V1_0;
CCFileStruct.MemorySize = ( ST25DVXXKC_MAX_SIZE / 8 ) & 0xFF;
CCFileStruct.TT5Tag = 0x05;
/* Init of the Type Tag 5 component (M24LR) */
while( NfcType5_TT5Init( ) != NFCTAG_OK );
}
/* Init done */
NFC07A1_LED_Off( GREEN_LED );
HAL_Delay( 300 );
NFC07A1_LED_Off( BLUE_LED );
HAL_Delay( 300 );
NFC07A1_LED_Off( YELLOW_LED );
HAL_Delay( 300 );
/* write text message to EEPROM */
K_Temperature= MAX6675_ReadTemperature(); //读�?�热电�?�温度值
HAL_Delay(1000);
// 将浮点数转�?�为字符串
char temp_str[20];
sprintf(temp_str, "%f", K_Temperature);
// 将字符串转�?�为无符�?�8�?整数数组
uint8_t temp_data[strlen(temp_str)];
memcpy(temp_data, temp_str, strlen(temp_str));
// 写入NDEF消�?�
NDEF_WriteNDEF(strlen(temp_str), temp_data);
//读�?�NDEF消�?�
NDEF_ReadNDEF(temp_data);
/* Set the LED3 on to indicate Programing done */
NFC07A1_LED_On( YELLOW_LED );
}