Skip to main content
Visitor II
April 16, 2019
Solved

The dynamic range of phase change in an RU3993

  • April 16, 2019
  • 2 replies
  • 798 views

Hi,

I am using one of the evaluation boards to test 3993. My objective is to determine the change in the phase of the reflected signal. For this reason, I use the movement detection mode that shows the Phase of the tag using the linear I & Q RSSI values.

My tag is attached with a phase shifter that shifts the phase of the reflected back signal. The shifter can be adjusted to delay the signal from 0 up to 100 degrees. Which I can confirm using a VNA of even Oscilloscope.

When operating in the system, where I use Reader to determine the phase of the reflected signal, from my tag which has a phase shifter attached with, I don't see as much phase delay as I can see on the VNA. The maximum phase change that I see is 5 degrees, which was expected to be instead 80 degrees. There are some configurations of distance/pathloss, gain of transmitted signal, sensitivity of the receiver and AGC mode where I get more dynamic range of up to 30 degrees. However, that is a very impractical case.

I have tried calibrating and turning on AGL mode as well, which sometimes show some improvements, however, a small increase or decrease in the pathloss kills the dynamic range of the phase detector at the reader.

I am unable to determine the reason behind this. Can someone please help me in resolving this issue? Should you need any further clarifications, please don't hesitate to ask.

Thanks in advance.

    This topic has been closed for replies.
    Best answer by Bart Herse

    Hello Nkhalid,

    you mention the movement detection mode - which GUI version and FW version are you running with the EVAL board?

    Note that from the IC you will be able to see a maximum of 90° phase change. In addition you should observe the phase bit which indicates if I and Q are in-phase or in anti-phase.

    Cheers,

    B

    2 replies

    Visitor II
    April 29, 2019

    Hello Nkhalid,

    you mention the movement detection mode - which GUI version and FW version are you running with the EVAL board?

    Note that from the IC you will be able to see a maximum of 90° phase change. In addition you should observe the phase bit which indicates if I and Q are in-phase or in anti-phase.

    Cheers,

    B

    NKhalAuthor
    Visitor II
    July 10, 2019

    Hi Bart,

    Thank you for your reply.

    I found that the problem was with my system. I was able to solve it by making some changes in it.

    On the other hand, I found the phase bit to be very unstable. moreover, the value it shows is usually wrong. Especially when we are approaching 10 degrees or 80 degrees. I can anticipate this by changing the frequency and observing if the phase increases or decreases to see if one is leading or lagging. Is there a way to make it more stable?