the write speed is too slow when writing date into Half-duplex 256 bytes dedicated buffer
hello sir
I am using the fast transmission mode of the nfc chip ST25DV04KC to transmit picture data. The NFC chip is used with the MCU of STM32G071G8U6. When I write the 25KB picture data through the mobile APP into the NFC cache, I find that the entire writing time takes about 11 seconds. Please tell me know, Is the transmission and writing time normal? If not, what is the error? If normal, is there any other chip or solution that can replace it? I need to control the entire time within 4 seconds
Thank you.