Tips on using wire wound Inductor as ST25DV antenna.
Hello,
Looking to integrate the ST25 in an ultra space constrained environment. As such antenna space is very limited so it seems like the best solution would be a wire wound inductor as read distance is not supercritical.
The Pulse W3102 4.7uH inductor seems to be designed to be a NFC antenna. What are somethings I should keep in mind when integrating this as the ST25DV antenna? Will any additional tuning components be need? Would any wirewound 4.7uH inductor work? 4.7uH seems to be a fairly common value for NFC wirewound antennas, why is that?
Additionally due to some of the safety requirements for this device there may be a design constraint to keep this inductor at 1uH or below. Preliminary research seems to indicate that a 1uH NFC should still be fine (?) . Could integrating a 1uH inductor work? What tuning components will be needed (at least to try as a first pass) ?
Thanks.