Using a PAIR of coils with a NFC transceiver
Today I have a project/board which uses the ST25R3911B NFC transceiver from ST, and it uses a dual layer coil (made of PCB copper traces) on the RF part. This coil is dual layer, that is, is a SINGLE coil made on the 2 sides of the board.
But I have a new situation/project where I want to have 2 (TWO/DUAL) coils connected to the NFC transceiver, and these coils would be separated with around 6 centimeters apart (one coil reads each side of the thing). They would be placed connected in parallel with their pair of wires... Is that possible? Is there a NFC transceiver from ST which can drive/read 2 independent coils? What can be done engineers? Or do I need to use a pair of transceivers?
Regards,
Jeferson.