Using ST25R3911B-DISCO
How can i use the ST25R3911B-DISCO without the GUI of ST?
Maybe with the help of the Framework, but how can I use the code or is there any documentation, because i can not found any.
How can i use the ST25R3911B-DISCO without the GUI of ST?
Maybe with the help of the Framework, but how can I use the code or is there any documentation, because i can not found any.
Hi,
ST25R3911B-DISCO is a ready-to-use kit with a PC GUI interacting with the embedded FW. The embedded FW needs to receive commands from a host (e.g. a PC with the GUI). If you want to not use the ST GUI, you need to provide your own application to send commands to the embedded FW. See Dll3911_Demos.sln for example of code on top of the ST25R3911B communication DLL: this can be used as a starting point for your own application.
If you are looking for a development board with a standalone FW, I would rather recommend to use the X-NUCLEO-NFC05A1 board and the X-CUBE-NFC5 FW package.
Feel free to provide more information about your application (i.e. is it a standalone application running on an MCU or a PC application).
Rgds
BT
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.