Using St25R3916B as NFC-V reader for ST25DV64KC
Hello everyone,
I am currently working with the ST25R3916B chip to use it as a reader for an ST25DV64KC tag. My objective is to interface with an NFC-V tag following the ISO 15693 standard.
To achieve this, I am developing custom code by referring to the examples provided by ST and consulting the datasheet. While someone suggested using the ST examples directly, I need a custom solution for my application.
So far, I have implemented all the initialization functions by closely following the "NFC08A1_PollingTagDetect" example, specifically the demoIni( ) function. Now, I am working on the application side and have been analyzing the demoCycle( ) function in detail, but I am encountering some challenges.
As my focus is on NFC-V tags, I have dived deeper into functions like demoNfcv. While I understand its overall structure and purpose, I feel like I am missing some key details. For example, I am unclear about what happens between the initialization phase and the execution of demoNfcv (where the RF message frame is constructed for transmission).
Here are my main questions:
After initializing the chip and enabling the field using the direct command 0xC8 (NFC initial field ON), what should I expect when an NFC-V tag is brought near the reader?
How can I confirm that the tag has been detected and the system is ready to send an RF message? Should I monitor specific interrupts or follow a particular procedure? Is enabling the field sufficient for tag detection?Once the field is enabled and a tag is detected, can I immediately send the required commands (e.g., read/write), or are there additional registers or commands that must be configured/sent to ensure the reader is ready to transmit via the RF antenna?
In the demoNfcv function, the 0x25 command (Select command) is sent, which includes the tag's UID. Could you explain its purpose and whether it is mandatory for communication?
Are there any detailed guidelines or application notes that go beyond the provided examples to explain the polling process and sending commands to a tag using the ST25R3916B?
Alternatively, could you help point out any gaps in my current understanding or implementation and guide me toward successfully sending RF commands to a tag?
I apologize for the lengthy questions, but I am trying to fully grasp how to use the ST25R3916B. I find it significantly more complex compared to the ST25DV64KC, which was much simpler and more intuitive as a tag.
Any advice, guidance, or resources would be highly appreciated!