Using two X-NUCLEO-NFC08A1 with X-CUBE-NFC6
Hello everyone,
for my project, I need to read a tag in two different places. Currently I am using an X-Nucleo-NFC08A1. I would like to add an additional X-Nucleo-NFC08A1 reader.
The communication is done via SPI. What adjustments do I have to make in the X-Cube-NFC6 to include an additional slave. Theoretically the pins SCL, MISO and MOSI should be the same.
The selection of which reader should be addressed is only done via the cs pin.
Rgds