Hello Derek,
In general for this application i would recommend the ST25R3916(B).
Having the mux / relay between EMC filter and NFC IC bears the risk of EMC problems.
The RFO outputs quite a fast rectangular signal. Thinking about Fourier, the rectangular signal is build out of multiple sine waves at multiple frequencies. The EMC filter removes / attenuates all of them and only the 13.56MHz sine will pass.
From this perspective, putting your switching circuit after the EMC filter seems to me the safest approach. The Vpp voltage there will be also lower than the one at the Antenna. You can have different CP and CS in order to adapt the matching of the different antennas.
You would now have many possibilities.
- mux the differential signal after the EMC Filter (10x differential mux)
- use the IC single ended and use two mux connected to each branch (2x5x single ended mux)
- like 2 but use the 50Ohm approach (cable + machting + 50Ohm antenna) (2x5x single ended 50Ohm mux) (https://eds.st.com/nfc-tuningcircuit/ => ST25R3916 - single ended with cable)
To have less losses, your mux should be as low ohmic as possible.
You could try to connect the RFI between series cap and the EMC filter. You then would not need to switch the Rx path.
In my opinion, 2 and 3 are the most reason ways to go. 3 is for sure the most expensive one (due to the 50ohm coaxial cable) but most likely the most reliable one.
Approach number 2 should also work and there should be a big quantity of mux available. You can also build your own, based on relays. Best would be if the mux is not loading the antenna, if it is not selected (coupling and loading between selected antenna and un-selected antenna nearby).
Hopefully i answered all your questions.
br Travis