What is the Proper Select sequence for ISO14443A with CR95HF?
I am using an arduino using SPI to communicate with a CR95HF.
I can ready the device ID and can detect a Mifare classic card in the RF field.
The problem I have is that I'm unable to select the card and have it respond with the SAK and CRC. All I get is an 87 response from the CR95HF.
Below is the data exchange.
To CR95HF>>>
From CR95HF <<<
>>> 00 04 02 26 07 (Detect card)
<<< 80 05 04 00 28 00 00 (Card response - no collision bit set)>>> 00 04 03 93 20 08 (start Collision loop to get UID for select)<<< 80 08 5B 48 66 3F 4A 28 00 00 (card responds with full UID)>>> 00 04 07 93 70 5B 48 66 3F 08 46 7B (SEL)<<< 87 00 (timeout?)What am I missing here?