Which is the best way to output max power?
Hello everyone,
I would really like to use the X-NUCLEO-NFC06A1 expansion board in order to transmit power wireless. I read that it should be able to transmit 1.6W of power.
At the moment I used the NFC06A1 available library to power up the board. In particular I called the rfalNfcInitialize(), rfalNfcDiscover() and rfalFieldOnAndStartGT(), functions.
This way I am able to see that the antennas are functioning properly, but i did some testing and it seems like i can only get very few mA from a receiving antenna.
Which is the best way to initialize the board in order to deliver maximum power (regarderless of circumstances)?
Thank you very much.