x-nucleo-nfc08a1, card emulator mode
I'm using X-NULCEO-NFC08A1 with NUCLEO-L476RG and sw sdk X-CUBE-NFC6 (project X-CUBE-NFC6\Projects\NUCLEO-L476RG\Applications\NFC08A1_PollingTagDetect).
I'm using an IPHONEX (ios16.5) with a custom app that writes nfc tag (but I've also tried the freeware version of app NFCTool available on the store).
The ST25R3916B should act as CARD EMULATOR and READER (both modes...but I've problems in CARD EMUL. mode)
Everything well, till when the data size written is lower than 90-100bytes...BUT when I try to write (from IPHONE to X-NUCLEO) a tag with bigger data size (for example 150bytes), it happens that last bytes (for example the bytes from 130 to 150) are written over the first bytes of the buffer.
I've spent many days to reselve this issue without succes. any hints ?
may I have the sw project NFC08A1_PollingTagDetect already configured to perform this task ?
thanks