Skip to main content
Explorer
July 2, 2025
Solved

Card Emulation (CE) NFC-V ST25R3918

  • July 2, 2025
  • 1 reply
  • 272 views

Hello ST Community,

I found this forum and the example code to our custom hardware very helpful and are successfully reading both NFC-A/NFC-V and emulating NFC-A on ST25R3918.

During testing, I've noticed that NFC-V tags with NDEF messages can also trigger background reads on both iOS and Android. Since NFC-V have longer ranges, would it be better to do CE using this format? 

At the moment the code is using demoT4T to respond to readers in NFC-A CE (RFAL_NFC_LISTEN_TECH_A) in the rfalNfcDiscoverParam.

do
{
 rfalNfcWorker();
 
 switch( rfalNfcGetState() )
 {
 case RFAL_NFC_STATE_ACTIVATED:
 transceiveBlocking( NULL, 0, &rxData, &rcvLen, &err, 0, false);
 break;
 
 case RFAL_NFC_STATE_DATAEXCHANGE:
 case RFAL_NFC_STATE_DATAEXCHANGE_DONE:
 txLen = demoCeT4T( rxData, *rcvLen, txBuf, sizeof(txBuf));
 transceiveBlocking( txBuf, txLen, &rxData, &rcvLen, &err, RFAL_FWT_NONE, false );
 break;
 
 case RFAL_NFC_STATE_START_DISCOVERY:
 return;
 
 case RFAL_NFC_STATE_LISTEN_SLEEP:
 default:
 break;
 }
}
while( (err == RFAL_ERR_NONE) || (err == RFAL_ERR_SLEEP_REQ) );

Is there sample code where I can push NDEF messages to NFC-V tags? How hard is it to implement and would it be worth the additional range (if there is any)?

Kind Regards,
Maximilian 

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

ST25R3918 natively supports card emulation for NFC-A and NFC-F technologies. The RFAL includes definitions for listening in NFC-A, NFC-B, NFC-F, and NFC-AP2P and manages card emulation in NFC-A and NFC-F.

Some customer applications, such as Flipper Zero, have implemented an ISO/IEC 15693 card emulation using the ST25R3916 stream mode or transparent mode. See the Flipper Zero firmware source code on GitHub.

I cannot comment on additional reading distance.

Regards,
BT

1 reply

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
July 2, 2025

Hi,

ST25R3918 natively supports card emulation for NFC-A and NFC-F technologies. The RFAL includes definitions for listening in NFC-A, NFC-B, NFC-F, and NFC-AP2P and manages card emulation in NFC-A and NFC-F.

Some customer applications, such as Flipper Zero, have implemented an ISO/IEC 15693 card emulation using the ST25R3916 stream mode or transparent mode. See the Flipper Zero firmware source code on GitHub.

I cannot comment on additional reading distance.

Regards,
BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.