Skip to main content
TChau.1
Associate II
August 17, 2021
Solved

Connection between STEVAL-SMARTAG1 and ST Link V2. Not able to detect the target board.

  • August 17, 2021
  • 5 replies
  • 1025 views

I am using STEVAL-SMARTAG1 and ST Link V2 (https://www.st.com/en/development-tools/st-link-v2.html)

Find the connections in the image attached.

Please share details related to required connections, debugger configuration etc.

0693W00000D2k66QAB.jpg

This topic has been closed for replies.
Best answer by TChau.1

Hi,

Initially we connected it using the flat ribbon cable. Now we connected directly with jumper cables and it got connected.

Thanks for pointing out.

We can mark this thread as close.

5 replies

Brian TIDAL
Technical Moderator
August 17, 2021

Hi TChau.1,

have you properly followed the various steps described in §7 of UM2427, in particular step #1 "Insert a CR2032 battery in the battery holder on the back of the STEVAL-SMARTAG1 evaluation board to power the target microcontroller."?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TChau.1
TChau.1Author
Associate II
August 18, 2021

Hello,

We are following the UM2427 document, but the document shows the connections for debugger based on Nucelo development board and we are using the ST-Link/V2 (Find the image_1). Does this debugger supports this Board/microcontroller.

  • Yes, Step #1 is followed. CR2032 is connected.
  • With STM32 Cube Programmer, we are testing the setup and getting the following logs/error. (Refer image_2)
  • We tried with multiple combinations of Port(SWD/JTAG), Frequency, Mode and Reset Mode. Please suggest expected configuration.

Image_1 : 

0693W00000Dpe1XQAR.pngImage_2 :

0693W00000Dpe1cQAB.png

Brian TIDAL
Technical Moderator
August 18, 2021

Hi,

I see no reason to have STLink/V2 not supporting this MCU. It should work in SWD configuration.

Have you connected the STEVAL-SMARTAG1 to the STLink/V2 flat ribbon or directly on the STLink/V2 PCB 20 pins connector? Can you check that the connection is not "mirrored" ?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TChau.1
TChau.1AuthorBest answer
Associate II
August 18, 2021

Hi,

Initially we connected it using the flat ribbon cable. Now we connected directly with jumper cables and it got connected.

Thanks for pointing out.

We can mark this thread as close.

Brian TIDAL
Technical Moderator
August 18, 2021

Well done! Thanks for your feedback.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.