Skip to main content
Associate
July 22, 2024
Solved

CR95HF DLL for x64

  • July 22, 2024
  • 1 reply
  • 1346 views

Good morning, I'm looking for the sources of the USB communication library for the CR95HF DLL, unfortunately the downloadable library is only for 32 bit systems, I would need the sources to be able to compile it at 64bit and eliminate the problem.
Can anyone help me solve my problem?

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

The source code of the CR95HF DLL 32-bits version will be provided to you in private.

Rgds

BT

 

1 reply

Brian TIDAL
Technical Moderator
July 23, 2024

Hi,

if I am not wrong, the CR95HF DLL has been ported to 64 bits inside the Software Development Kit for ST25  (STSW-ST25SDK001) in ST25SDK-1.11.0\readers\st\resources\windows\x64.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
July 23, 2024

Hi, 

The DLL is 64 bit, the problem now is that the exported functions do not coincide with those present in the old one.

Like:

CR95HFDLL_USBconnect

CR95HFDLL_USBhandlecheck

CR95HFDLL_getHardwareVersion

And all other function if i dump exported function:

Dump of file cr95hf.dll

File Type: DLL

Section contains the following exports for cr95hf.dll

00000000 characteristics
592E8352 time date stamp Wed May 31 10:48:18 2017
0.00 version
1 ordinal base
10 number of functions
10 number of names

ordinal hint RVA name

1 0 00001E70 Java_com_st_st25pc_model_rfReaders_st_STReader_antiCollision
2 1 00001500 Java_com_st_st25pc_model_rfReaders_st_STReader_connect
3 2 000015E0 Java_com_st_st25pc_model_rfReaders_st_STReader_disconnect
4 3 000014F0 Java_com_st_st25pc_model_rfReaders_st_STReader_echo
5 4 000015F0 Java_com_st_st25pc_model_rfReaders_st_STReader_getName
6 5 000015D0 Java_com_st_st25pc_model_rfReaders_st_STReader_isConnected
7 6 00001640 Java_com_st_st25pc_model_rfReaders_st_STReader_selectReaderMode
8 7 00002060 Java_com_st_st25pc_model_rfReaders_st_STReader_sendPps
9 8 00001FA0 Java_com_st_st25pc_model_rfReaders_st_STReader_sendRats
10 9 00001950 Java_com_st_st25pc_model_rfReaders_st_STReader_sendReceive

I can't find any reference to the old APIs of the previous version, this one seems like a totally different version.

Thanks

 

 

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
July 24, 2024

Hi,

The source code of the CR95HF DLL 32-bits version will be provided to you in private.

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.