Skip to main content
DJeon.4
Associate III
July 18, 2022
Solved

CR95HF mifareCard 1k memory Read Write method?

  • July 18, 2022
  • 2 replies
  • 1758 views

​Hello, I am developing Arduino using CR95HF.

I succeeded in reading the Tag ID using Cr95HF

If you read it with mifareCard 1K, you can read the Tag ID, but it does not read/write the memory sector.

I need to go through the authentication method to read, but I would appreciate it if you could tell me how to use it because there is no description. Can you provide the data informally?

Thank you.0693W00000QLOkdQAH.png

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi,

    see similar post on this subject: https://community.st.com/s/question/0D53W00000Gj4noSAB/hellocan-any-one-write-a-block-data-into-1k-mifare-classic-card-with-cr95hf-isoiec14443athanks

    Such tag use proprietary authentication and ciphering. CR95HF supports the physical framing used for those tags. The support of the proprietary authentication and ciphering on top of CR95HF cannot be provided by ST for legal reasons.

    Such tags are not Type 2 compliant. If your want to simply perform Read/Write commands, Type 2 compliant tags will fulfill your need: I would recommend to use T2T tags from the ST25TN series.

    Rgds

    BT

    2 replies

    Brian TIDAL
    Brian TIDALBest answer
    Technical Moderator
    July 18, 2022

    Hi,

    see similar post on this subject: https://community.st.com/s/question/0D53W00000Gj4noSAB/hellocan-any-one-write-a-block-data-into-1k-mifare-classic-card-with-cr95hf-isoiec14443athanks

    Such tag use proprietary authentication and ciphering. CR95HF supports the physical framing used for those tags. The support of the proprietary authentication and ciphering on top of CR95HF cannot be provided by ST for legal reasons.

    Such tags are not Type 2 compliant. If your want to simply perform Read/Write commands, Type 2 compliant tags will fulfill your need: I would recommend to use T2T tags from the ST25TN series.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    DJeon.4
    DJeon.4Author
    Associate III
    July 18, 2022

    Thank you for your answer.

    Could you share the data on how to activate the CR95HF card emulator function? I would appreciate it if you could share the code data informally.

    I am developing by applying CR95HF with Arduino sketch.

    ST Employee
    July 19, 2022

    Question edited by moderation - Please, do not post private info on public posts

    DJeon.4
    DJeon.4Author
    Associate III
    July 20, 2022

    I'll be careful. Thank you.