Skip to main content
DSai.1
Associate III
August 17, 2022
Solved

declaration of BSP_SPI1_IRQ_Callback() in FreeRTOS_polling

  • August 17, 2022
  • 22 replies
  • 6622 views

about declaration of BSP_SPI1_IRQ_Callback() in ST25NFC_Embedded_Lib_ST25R3916_1.4.0\Projects\STM32L476RG-Nucleo\Applications\X-NUCLEO-NFC06A1\FreeRTOS_polling

Dear Sir,

I am check the process flow of sample program which use FreeTROS.

I found that the function BSP_SPI1_IRQ_Callback() is declared in two place,

one is in nucleo_l476rg_bus.c, another is in plf_adaptation.c .

Could you tell me which one is used in this demo sample?

Also, in this sample code, st25r3916Isr() is called in two different place.

one is in

----------------------------------------

void nfcIsrTaskRunner(void *argument)

{

 /* Infinite loop */

 for(;;)

 {

   ulTaskNotifyTake( pdTRUE, portMAX_DELAY );       /* Check if IRQ happen execute immediately, otherwise other execute Task meanwhile */

   st25r3916Isr();                     /* ISR called from main task avoid calling vTaskSuspendAll from ISR (SPI) - NFC IRQ pin is anyhow checked */

   xSemaphoreGive(platformSem);

 }

}

-------------------------------------------------------

another is in

--------------------------------------

__weak void BSP_SPI1_IRQ_Callback(void)

{

 /* Prevent unused argument(s) compilation warning */

  

 /* This function should be implemented by the user application.

  * It is called into this driver when an event from ST25R3916 is triggered. 

  */

 st25r3916Isr();

}

---------------------------------------

Are there two manners used in this demo? What are the main differences for them?

Best regards

Dai Sai

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

As the initial issue described in this post is fully solved, I would suggest to create a new post dedicated to the CRC issue on Read Multiple Block. I would recommend as well to share information about the tag manufacturer and tag model. Make sure to define a big enough rxBuf (should 1 byte for response flag + 2 bytes for CRC + blockSize * number of requested blocks). Note that the CRC is present in the buffer after the data. Also, blockNum should be 1 when requesting to read 2 blocks.

Rgds

BT

22 replies

DSai.1
DSai.1Author
Associate III
August 18, 2022

Dear sir

After I read code, It seems the following code is used in demo sample.

void nfcIsrTaskRunner(void *argument)

{

 /* Infinite loop */

 for(;;)

 {

   ulTaskNotifyTake( pdTRUE, portMAX_DELAY );       /* Check if IRQ happen execute immediately, otherwise other execute Task meanwhile */

   st25r3916Isr();                     /* ISR called from main task avoid calling vTaskSuspendAll from ISR (SPI) - NFC IRQ pin is anyhow checked */

   xSemaphoreGive(platformSem);

 }

}

Also, BSP_SPI1_IRQ_Callback() that is declared in in plf_adaptation.c is used.

My understand are correct?

By the way, I have another question.

In void StartDefaultTask(void *argument), demoCycle() is called.

But I found there are several version for demoCycle(). Could you tell me the

path for demoCycle() that is used here. I want to verify demo for ISO15693.

The demo sample code ( FreeRTOS_polling ) I referred can be used for

ISO15693 by modifying platform.h only?

best regards

Dai Sai

DSai.1
DSai.1Author
Associate III
August 18, 2022

Dear Sir,

May I use demoInit() and democycle() declared in T25NFC_Embedded_Lib_ST25R3916_1.4.0\Projects\STM32L476RG-Nucleo\Applications\X-NUCLEO-NFC06A1\FTM\Src\ftm_poller.c?

best regards

Dai Sai

Ulysses HERNIOSUS
Technical Moderator
August 18, 2022

Hi Dai Sai,

the actual used demoCycle() can be seen from the project you are using - worst case you can verify from map file the actual linked version.

There are various demoCycle implementations depending on the type of demo.

I think similar for the BSP_SPI1_IRQ_Callback(), the project should define which one is compiled/used. I think a different one is used whether you are compiling one of the bare-bone demos or the FreeRTOS demo.

If not clear, please ask again, a colleague of mine can have next week a look.

Best Regards, Ulysses

DSai.1
DSai.1Author
Associate III
August 18, 2022

Dear Ulyssesk

thank you very much for your reply.

Because the tool ST25R3916-DISCO is not available from dealer in Japan,

I don't have compiling environment.

With my current environment, I can not confirm which implementation is used.

If possible, I hope you can give me information about these functions.

If so, we can port the driver faster.

I am porting the code for my ThreadX environment. Here I use a X-NUCLEO-NFC06A1

connecting to my SoC.

best regards

Dai Sai

DSai.1
DSai.1Author
Associate III
August 18, 2022

Dear Ulyssesk,

I wrote a version for demoInit() and demoCycle() for testing the basic accessing function of ISO15693 card as following

bool rfal_demoIni(void)

{

ReturnCode err;

err = rfalNfcInitialize();

if (err == ERR_NONE)

{

discParam.compMode = RFAL_COMPLIANCE_MODE_NFC;

discParam.devLimit = 1U;

discParam.nfcfBR = RFAL_BR_212;

discParam.ap2pBR = RFAL_BR_424;

discParam.notifyCb = demoNotif;

discParam.totalDuration = 1000U;

discParam.wakeupEnabled = false;

discParam.wakeupConfigDefault = true;

discParam.techs2Find = RFAL_NFC_POLL_TECH_V;

state = DEMO_ST_START_DISCOVERY;

return true;

}

return false;

}

////////////////////////////////////////////////////////////////////////////////////////////////

void rfal_demoCycle(void)

{

static rfalNfcDevice *nfcDevice;

rfalNfcWorker();                  /* Run RFAL worker periodically */

#if 0

/*******************************************************************************/

/* Check if USER button is pressed */

if (BSP_PB_GetState(BUTTON_USER) == GPIO_PIN_RESET)

{

discParam.wakeupEnabled = !discParam.wakeupEnabled;  /* enable/disable wakeup */

state = DEMO_ST_START_DISCOVERY;            /* restart loop     */

platformLog("Toggling Wake Up mode %s\r\n", discParam.wakeupEnabled ? "ON" : "OFF");

/* Debounce button */

while (BSP_PB_GetState(BUTTON_USER) == GPIO_PIN_RESET);

}

#endif 

discParam.wakeupEnabled = true;  /* enable/disable wakeup */

state = DEMO_ST_START_DISCOVERY;            /* restart loop     */

//tx_thread_sleep(OS_MSECS_TO_TICKS(2000));

switch (state)

{

/*******************************************************************************/

case DEMO_ST_START_DISCOVERY:

rfalNfcDeactivate(false);

rfalNfcDiscover(&discParam);

state = DEMO_ST_DISCOVERY;

break;

/*******************************************************************************/

case DEMO_ST_DISCOVERY:

if (rfalNfcIsDevActivated(rfalNfcGetState()))

{

rfalNfcGetActiveDevice(&nfcDevice);

switch (nfcDevice->type)

{

/*******************************************************************************/

/*******************************************************************************/

case RFAL_NFC_LISTEN_TYPE_NFCV:

{

uint8_t devUID[RFAL_NFCV_UID_LEN];

ST_MEMCPY(devUID, nfcDevice->nfcid, nfcDevice->nfcidLen);  /* Copy the UID into local var */

//REVERSE_BYTES(devUID, RFAL_NFCV_UID_LEN);         /* Reverse the UID for display purposes */

//platformLog("ISO15693/NFC-V card found. UID: %s\r\n", hex2Str(devUID, RFAL_NFCV_UID_LEN));

//platformLedOn(PLATFORM_LED_V_PORT, PLATFORM_LED_V_PIN);

demoNfcv(&nfcDevice->dev.nfcv);

}

break;

/*******************************************************************************/

default:

break;

}

rfalNfcDeactivate(false);

platformDelay(500);

state = DEMO_ST_START_DISCOVERY;

}

break;

/*******************************************************************************/

case DEMO_ST_NOTINIT:

default:

break;

}

}

////////////////////////////////////////////////////////////////////////////////////

The rfal_demoCycyle() will be called at the same style of nfcStartDefaultTask(void *argument) in FreeRTOS_polling package. The following is my code.

----------------------------------------------

void ddi_Rfal_Tag_Rx_Thread(ULONG param)

{

//tx_thread_sleep(10);

tx_thread_sleep(OS_MSECS_TO_TICKS(1000));

//initialize the RFAL NFC ??? 

rfal_demoIni();

while (1)

{

rfal_demoCycle();

tx_semaphore_get((TX_SEMAPHORE_PTR)&g_pRfalSemaSt25r3916IRQ);

}//while

}

---------------------------------------------

Are there any problem?

Best regards

Dai Sai

Brian TIDAL
Technical Moderator
August 22, 2022

Hi,

BSP_SPI1_IRQ_Callback definition in nucleo_l476rg_bus.c has the __weak attribute. Therefore, this definition is overridden by the one in plf_adaptation.c.

BSP_SPI1_IRQ_Callback notifies the ISR thread (nfcIsrTaskRunner) to process the ST25R3916 IRQ by calling st25r3916Isr().

Make sure to have the IRQ properly handled in your porting.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DSai.1
DSai.1Author
Associate III
August 23, 2022

Dear Brian,

thank you very much for your reply.

I have the same idea with you. I ported the code based on the code in plf_adaptation.c.

Today, I did the rfalinitialize() and rfalFieldOnAndStartGT() with my ThreadX environment,

and got the a strong RF carrier, which is much stronger than one I did with TRF7960 before.

I was a little exciting for the good first step. I will try to read out UID of ISO15693 next try.

Attached figures is the IRQ and the output of RF carrier. Are they normal?0693W00000QOG8mQAH.png0693W00000QOG8cQAH.png 

Best regards

Dai Sai

DSai.1
DSai.1Author
Associate III
August 23, 2022

Dear Brian,

By checking the return value of rfalFieldOnandStartGT(), the return value is ERR_INTERNAL(12U).

I wonder if the return error should be checked at current stage?

best regards

Dai Sai

Brian TIDAL
Technical Moderator
August 23, 2022

Hi,

rfalFieldOnandStartGT should return ERR_NONE. I suspect an issue in the adaptation to the threadX platform, likely in the timer management.

I would suggest to enable ST25R_SELFTEST and ST25R_SELFTEST_TIMER as global defines in the compiler command line. Then check the return code of st25r3916Initialize called in rfalInitialize.:

  • ERR_NONE: interrupt, timer and serial communication with the ST25R3916 are OK
  • ERR_IO: serial communication issue (likely not the case here)
  • ERR_TIMEOUT: interrupt management issue
  • ERR_SYSTEM: timer issue (my best guess)

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DSai.1
DSai.1Author
Associate III
August 23, 2022

Dear Brian,

thank you very much for your comment.

The return code from rfalinitialize() is ERR_NONE(0).

I will try what you suggested.

best regards

Dai Sai