Skip to main content
Jhern.1
Associate III
July 7, 2020
Solved

Differences between ST95HF and ST25R95

  • July 7, 2020
  • 12 replies
  • 4758 views

Hi,

I am assessing to use CR95HF, ST95HF or ST25R95 for a low power access control reader application and I have a question.

I would like to know if thre is any difference between thse 2 parts:

  • ST95HF
  • ST25R95

Regards, Ramon.

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi,

    you can use the STSW-95HF001  tag detection user interface or compile X-CUBE_NFC3 free of charge using STM32CubeIDE.

    For your information, the X-CUBE_NFC3 can be ported on other MCU including non ST MCU (as long as a ST reader device is used: see the licence agreement). The porting on other MCU can be achieved through the macros in platfom.h (only little effort needed)

    Rgds

    BT

    12 replies

    Brian TIDAL
    Technical Moderator
    June 2, 2023

    Hi,

    I would recommand not to post on an old and already answered thread (to avoid never ending thread) Feel free to enter a new thread.

    Rgds

    BT.

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Brian TIDAL
    Technical Moderator
    October 23, 2023

    Hi, 

    I would suggest to create a new thread rather that posting on an already answered thread. As far as I know the reset control byte is identical on CR95HF, ST95HF and ST25R95: 0x01 (see §4.1.1 in the ST25R95 datasheet). And no FW change is needed when moving from ST95HF to ST25R95. Feel free to create a new thread if you need more information.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.