Skip to main content
Schuyler
Associate III
October 19, 2023
Solved

How about STEVAL-SMARTAG1 No power mode?

  • October 19, 2023
  • 2 replies
  • 1117 views

Currently purchased with the STEVAL-SMARTAG1, it was discovered that the capability collected through the ST25 powers the L0 via EH pin VDD while collecting data from the sensor. I need to collect signals by thermocouple, which is the same transmission mode as SPI. Can I successfully collect data in this way? Any better suggestions?

This topic has been closed for replies.
Best answer by John TRAN

Hi there, The Smartag1 voltage rail is 1.8V in energy harvesting mode ( no battery). so there is no option for delivering 3.3V. 

Normally with a phone, the ST25DV will not deliver more than 3V @2mA. 

2 replies

Michael GALIZZI
ST Employee
October 24, 2023

Hello,

the EH pin provides a very limited current and a very unstable voltage. Therefore, an LDO is used to stabilize the voltage to the MCU to 1.8 V. The thermocouple (such as the MAX6675) requires higher operating voltage (3.0 V to 5.5 V) and an higher current than that the ST25 is able to provide.

Best regards,

Michael

Schuyler
SchuylerAuthor
Associate III
October 25, 2023

Hi, @Michael GALIZZI 

Yes, where VDD can wake up the mcu, but can not meet the MAX6675 requirements, then L0 has other 3.3v voltage? Can I design a voltage pin with a 3.3v output from the VDD voltage?

John TRAN
John TRANBest answer
ST Employee
December 4, 2023

Hi there, The Smartag1 voltage rail is 1.8V in energy harvesting mode ( no battery). so there is no option for delivering 3.3V. 

Normally with a phone, the ST25DV will not deliver more than 3V @2mA.