Skip to main content
Associate III
January 26, 2024
Solved

kill command does not work

  • January 26, 2024
  • 1 reply
  • 1151 views

Hi, 

It looks like the kill command is not working for ST25TV16K. I am getting an error command as shown below:

Luke_abc_0-1706284134858.png

The register values are given below:

Luke_abc_1-1706284167456.png

 

 

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

this menu is intended for tags supporting the Kill command such as ST25TV02K. 

For the ST25TV16K, the kill feature is supported through registers settings i.e. the kill feature is not achieved through a kill command but through settings in register 03h (see datasheet of this product).

Therefore, the GUI behaves accordingly as the ST25TV16K dos not support the kill command. Make sure to use the registers menu in case you want to use the kill feature on ST25TV16K.

Rgds

BT

 

1 reply

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
January 30, 2024

Hi,

this menu is intended for tags supporting the Kill command such as ST25TV02K. 

For the ST25TV16K, the kill feature is supported through registers settings i.e. the kill feature is not achieved through a kill command but through settings in register 03h (see datasheet of this product).

Therefore, the GUI behaves accordingly as the ST25TV16K dos not support the kill command. Make sure to use the registers menu in case you want to use the kill feature on ST25TV16K.

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.