Layout Recommendations for ST3916 and ST3918
We are currently seeking layout recommendations for the ST25R3916 and ST25R3918 chips.
On the Transmitter Side:
ST25R3916B → Power Amplifier → Matching Circuit → Antenna
On the Reciever Side:
Antenna → Matching Circuit →Power Harvester → ST25R3918
- The implemented power amplifier is a Class E amplifier configured in push-pull mode (We intend to transmit power along with NFC communication)
- The matching circuit has been designed using the ST25R Antenna Matching Tool.
- We are using a differential configuration, and as such, the matching elements have been placed symmetrically on both arms.
- A provision for a balun has been included between the power transmitter and the matching network.
We have the following queries:
- The ST25R Antenna Matching Tool provides both single-ended and differential matching options. For the single-ended configuration, we understand that the PCB trace impedance should be matched to 50 ohms, whereas for the differential configuration, the PCB traces should follow 100-ohm differential routing.Could you please confirm if this understanding is correct?
- If we choose the differential configuration, should the entire signal path—from the ST25R3916 to the antenna—be routed with 100-ohm differential impedance?
- Are there any application notes from ST regarding power amplifier design? At present, we have designed the amplifier based on standard Class E equations and have simulated the circuit in LTspice. However, if there are any specific resources or recommendations from ST, we would be grateful if you could share them.