Skip to main content
hhest.1
Associate
September 14, 2022
Solved

M24SR02-Y not working after writing NDEF message via I2C to it

  • September 14, 2022
  • 4 replies
  • 1091 views

After writing a NDEF message to the M24SR02-Y NFC Tag the Chip doesn't work anymore. If I scan it with a NFC app I can see that under technologies NDEF isn't listed anymore. Before the writing process it was listed. Does anybody know a reason for this?

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

you probably try to write a bluetooth record with mine type = application/vnd.bluetooth.ep.oob but your buffer seems corrupted with a 00 every 2 bytes (it looks like a Double Byte Char String issue). So the NDEF message inside the tag memory is inconsistent. Using the  ST25 NFC Tap, you can go to the MEMORY tab and see that the content of the NDEF is incorrect.

Rgds

BT

4 replies

Brian TIDAL
Technical Moderator
September 14, 2022

Hi,

can you use the ST25 NFC Tap app and provide the information returned by the app after the NDEF Write? Also, make sure to have the I2C token being released before starting an RF session (see M24SR02-Y datasheet §4.2).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
hhest.1
hhest.1Author
Associate
September 14, 2022

0693W00000SvNMpQAN.jpg0693W00000SvNN4QAN.jpg0693W00000SvNNOQA3.jpg0693W00000SvNNTQA3.jpgThis are the informations the app gets from the tag. To close the I2C session I just turn off the supply voltage of the tag.

The NDEF file seems to be empty, but during communication via I2C I get "command completed as response. Here is the whole writing process:

write to 0x56 ack data: 0x26 0xCA 0x15 

write to 0x56 ack data: 0x02 0x00 0xA4 0x04 0x00 0x07 0xD2 0x76 0x00 0x00 0x85 0x01 0x01 0x00 0x35 0xC0 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xA4 0x00 0x0C 0x02 0x00 0x01 0x3E 0xFD 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x01 0x01 0x65 0x9C 0x03 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x02 0x02 0xD2 0x00 0x29 0xE3 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x04 0x02 0x20 0x00 0x0B 0xE7 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x06 0x02 0x61 0x00 0xC3 0x81 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x08 0x02 0x70 0x00 0xC8 0xA3 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x0A 0x02 0x69 0x00 0x37 0xD8 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x0C 0x02 0x61 0x00 0x6D 0x5D 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x0E 0x02 0x69 0x00 0xDB 0xAA 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x10 0x02 0x6E 0x00 0x30 0x8A 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x12 0x02 0x76 0x00 0x17 0xE8 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x14 0x02 0x64 0x00 0xAC 0x05 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x16 0x02 0x62 0x00 0x0A 0x68 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x18 0x02 0x75 0x00 0xD1 0x1E 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x1A 0x02 0x74 0x00 0x7F 0x3E 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x1C 0x02 0x6F 0x00 0xDC 0x04 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x1E 0x02 0x68 0x00 0xA2 0x70 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x20 0x02 0x6C 0x00 0x72 0xF5 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x22 0x02 0x2E 0x00 0xD2 0xB9 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x24 0x02 0x6F 0x00 0xF6 0xAD 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x26 0x02 0x08 0x00 0xDD 0xBC 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x28 0x02 0xA9 0x00 0xB8 0xA4 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x2A 0x02 0xD4 0x00 0x72 0xDD 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x2C 0x02 0x00 0x00 0xB3 0xAE 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x2E 0x02 0x00 0x00 0xC5 0x97 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x30 0x02 0x1C 0x00 0x17 0xC6 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x32 0x02 0x11 0x00 0x19 0x4F 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x34 0x02 0x9D 0x00 0xEF 0x21 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x36 0x02 0xB5 0x00 0x6A 0xF5 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x38 0x02 0x00 0x00 0xFE 0x1F 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x3A 0x02 0x00 0x00 0x88 0x26 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x3C 0x02 0x00 0x00 0x12 0x6D 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x3E 0x02 0x00 0x00 0x64 0x54 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x40 0x02 0x00 0x00 0x63 0xA0 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x42 0x02 0x00 0x00 0x15 0x99 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x44 0x02 0x11 0x00 0xC6 0x5E 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x46 0x02 0x6D 0x00 0xD4 0x3E 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x48 0x02 0xF6 0x00 0x63 0x6D 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x4A 0x02 0xC3 0x00 0x0F 0x9C 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x4C 0x02 0xB6 0x00 0xE9 0x59 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x4E 0x02 0x45 0x00 0xFF 0x36 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x50 0x02 0xE0 0x00 0x5B 0x8A 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x52 0x02 0xB2 0x00 0x6A 0x53 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x54 0x02 0xE8 0x00 0x77 0x36 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x56 0x02 0x03 0x00 0x30 0x02 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x58 0x02 0x00 0x00 0x1A 0x86 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x5A 0x02 0x0D 0x00 0x14 0x0F 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x5C 0x02 0x48 0x00 0x50 0x7C 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x5E 0x02 0x6C 0x00 0x75 0x01 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x60 0x02 0x6F 0x00 0xAD 0xC9 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x62 0x02 0x43 0x00 0x48 0x7A 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x64 0x02 0x69 0x00 0x91 0xEF 

read to 0x56 ack data: 0x02 0x90 0x00 0xF1 0x09

write to 0x56 ack data: 0x02 0x00 0xD6 0x00 0x66 0x01 0x6E 0x07 0x34 

read to 0x56 ack data: 0x03 0x90 0x00 0x2D 0x53

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
September 14, 2022

Hi,

you probably try to write a bluetooth record with mine type = application/vnd.bluetooth.ep.oob but your buffer seems corrupted with a 00 every 2 bytes (it looks like a Double Byte Char String issue). So the NDEF message inside the tag memory is inconsistent. Using the  ST25 NFC Tap, you can go to the MEMORY tab and see that the content of the NDEF is incorrect.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
hhest.1
hhest.1Author
Associate
September 15, 2022

Oh I see. I fixed the bug in my code and it is working now. Thank you very much for your help.