Skip to main content
Associate II
December 3, 2024
Solved

Mailbox Password Crash

  • December 3, 2024
  • 1 reply
  • 527 views

Hello,

 

I am trying to enable the Mailbox functionality on ST25DV64KC-DISCO board.

 

I am using the NFCTap project,

And inside it added my own storyboard and a View controller.

This view controller first detects a tag at launch in view didload,

then it fetches the mailbox status,

and lastly it tries to enable mailbox with presentpassword api on which it crashes.

 

I have also attached a screen cast.

Please let me know if anyone faced a similar issue and can advice a solution.

Screenshot 2024-12-03 at 14.24.54.png

This topic has been closed for replies.
Best answer by victor laraison

Hello aly,

Error message in your debug console is quite explicit: you 're not connected with the tag, and you try to send a command. So, you get an exception. 
So : 

- Verify why you re connected with tag (do you stop nfc session ? Distance from tag & reader too far ? ....)

- Catch your exeption by using the example provided in source code of NFC tap with the "SwitfTryCatch" class.

Hope it helps.

 

1 reply

victor laraison
victor laraisonBest answer
ST Employee
December 20, 2024

Hello aly,

Error message in your debug console is quite explicit: you 're not connected with the tag, and you try to send a command. So, you get an exception. 
So : 

- Verify why you re connected with tag (do you stop nfc session ? Distance from tag & reader too far ? ....)

- Catch your exeption by using the example provided in source code of NFC tap with the "SwitfTryCatch" class.

Hope it helps.