Skip to main content
ANaud.1
Associate III
June 16, 2021
Solved

MCU control the antenna function of ST25R3916

  • June 16, 2021
  • 2 replies
  • 1315 views

Is there a way to have any MCU control the antenna function of the ST25R3916, if we use the ST25R3917, as there is a stock shortage of the 3916 ?

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi ANaud.1,

I assume you are referring to AAT? AAT in ST25R3916 is implemented by two DACs providing a voltage to the control pins of variable capacitors.

You could do basically the same by using two other DACs (for example from your MCU if available). However there are some limitations with regards to power-down/wake-up mode - you may need to keep them active all the time or otherwise you may experience issues when using the inductive wake-up feature of St25R3916/7.

Best Regards, Ulysses

2 replies

Ulysses HERNIOSUS
Technical Moderator
June 17, 2021

Hi ANaud.1,

I assume you are referring to AAT? AAT in ST25R3916 is implemented by two DACs providing a voltage to the control pins of variable capacitors.

You could do basically the same by using two other DACs (for example from your MCU if available). However there are some limitations with regards to power-down/wake-up mode - you may need to keep them active all the time or otherwise you may experience issues when using the inductive wake-up feature of St25R3916/7.

Best Regards, Ulysses

TZhou.2
Associate II
September 14, 2021

Hi Ulysses,

As I know the ATT is an auto-tunning technology, but I'm not familiar with coding about this. Could you provide some tutorials about how to configure the ATT on NFC06A1 board?

Thanks,

Thomas

Ulysses HERNIOSUS
Technical Moderator
September 14, 2021

Hi Thomas,

please have a look at AN5322.

Best Regards, Ulysses

TZhou.2
Associate II
September 14, 2021

Hi Ulysses,

Thanks for your reply. But I have also another question: how to measure the energy efficiency parameter on NFC06A1 board? If I test the VDD_RF pin is helpful? Thanks,

Thomas