Skip to main content
Associate
February 12, 2025
Solved

Mifare Classic Authentication Failure on ST25R3916B

  • February 12, 2025
  • 2 replies
  • 2818 views

We are using an ST25R3916B  to read and write to both ST25TV512C tags and Mifare Classic 1K cards. While we have successfully communicated with ST25 tags, we are encountering issues at the authentication stage with Mifare Classic.

Steps We Are Following:

  1. Ensure Activation State

Before sending authentication commands, we ensure the reader is in the RFAL_NFC_STATE_ACTIVATED state.

  1. Send Authentication Command to Retrieve the 4-Byte Challenge

Mifare Classic authentication follows a challenge-response mechanism. To begin, we must send the authentication command and obtain a 4-byte random challenge from the card.

The command consists of:

  • Byte 0: Authentication command (0x60 for Key A, 0x61 for Key B).
  • Byte 1: Target block number.
  • Bytes 2-7: 6-byte key (Key A or Key B).
  • Bytes 8-11: Card UID (copied from the detected card structure).

uint8_t authCmd[12];

authCmd[0] = 0x60; // Authenticate using Key A

authCmd[1] = block; // Block number

memcpy(&authCmd[2], keyA, 6); // Copy the 6-byte key

memcpy(&authCmd[8], device.nfcid, device.nfcidLen); // Copy the UID

 

We then transmit this using rfalTransceiveBlockingTxRx():

status = driver.rfalTransceiveBlockingTxRx(

    authCmd,         // Transmit buffer

    sizeof(authCmd), // Transmit length

    response,        // Receive buffer

    sizeof(response), // Max receive length

    &responseLen,    // Actual response length

    RFAL_TXRX_FLAGS_DEFAULT,

    RFAL_FWT_NONE

);

  • If successful, the card should respond with a 4-byte challenge.
  • This challenge must be processed using the Mifare Classic 48-bit cipher to generate the authentication response.

Current Issue

In the code below, I attempt to send only 4 bytes for authentication, which includes CRC values (D1 and 3D) for 0x60 and 0x04:

uint8_t authCmd[4];

authCmd[0] = 0x60;  // Authentication command (Key A)

authCmd[1] = 0x04;  // Block number

authCmd[2] = 0xD1;  // CRC for 60 and 04

authCmd[3] = 0x3D;  // CRC

 

status = driver.rfalTransceiveBlockingTxRx(

    authCmd,         // Transmit buffer

    sizeof(authCmd), // Transmit length

    response,        // Receive buffer

    sizeof(response), // Max receive length

    &responseLen,    // Actual response length

    RFAL_TXRX_FLAGS_DEFAULT,

    RFAL_FWT_NONE

);

  • I receive ERR_IO (3), which is a generic I/O error.
  • Sometimes, I get ERR_TIMEOUT (4), but I believe ERR_IO is the root cause.

 

What I Need Help With

  • What RFAL calls should I use after reaching RFAL_NFC_STATE_ACTIVATED to retrieve the 4-byte challenge?
  • Am I correctly handling Mifare Classic authentication in RFAL?
  • Should I allow RFAL to handle CRC, or should I manually append it?
  • Any debugging suggestions for ERR_IO?

Any help would be greatly appreciated.

Thanks in advance.

 

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi,

please beware that for your target command to be accepted by the the card it needs to be in ACTIVE state. You need to go to ISO14443-A tab: Configuration + WUPA->Active. Then you can switch to Debug tab and execute one time a command as I had shown in my previous post.

You will not be able to repeat this command  or send the another command (even if not answered) - you need to go back to ISO14443-A tab and repeat the whole sequence.

With any unknown command the tag will fall out of its current state.

Of course if you receive a positive answer you could continue with the next well-formed command.

Not sure about your reference to REQA: This command (and WUPA) wakes a tag. It is not sufficient to move the tag into Active state. For the active state also the complete AC/Select procedure are required. This is what these buttons on ISO14443-A tab do.

BR, Ulysses

2 replies

Ulysses HERNIOSUS
Technical Moderator
February 13, 2025

Hi AMCI,

you can find some hints here: nfc0541-read-mifare-classic-1k .

Concerning the ERR_IO: No idea really, please debug through and isolate the code line. There should only be very few ERR_IO and in normal operation this error code shouldn't appear.

Regards, Ulysses

Visitor II
March 5, 2025

I have the same issue with not being able to receive the NONCE upon calling the code here.   After powering up the ST25R3916B, we set it to 3.3V in register 0x01H by setting bit 7 high Updated value of register 0x1 (Binary): 0b10000000.

With or without the register setting, I can successfully get the device, identify it as Mifare Classic 1K (ATQA: 04 00
SAK: 08) and then proceed to the authentication using the code below.

In some other threads, I read that I should be using bit-oriented calls vs. byte.  Does that apply to the call to which the device responds with the nonce.  I'm not able to get the nonce. My ESP32S3 MCU goes to watchdog and reboots.

bool CrNfc::authenticateMifareClassic(const rfalNfcDevice *device)
{
uint8_t authCmd[12] = {0}; // Authentication request
uint8_t response[4] = {0}; // Expected nonce response
uint16_t responseLen = 0;

authCmd[0] = 0x60;
authCmd[1] = 0x04 // Block address (first block in sector)

memcpy(&authCmd[2], mifareKey, 6);
if (device->nfcidLen < 4)
{
Serial.println(":cross_mark: Error: NFCID too short!");
return false;
}

memcpy(&authCmd[8], &device->nfcid[device->nfcidLen - 4], 4); // Last 4 bytes of NFCID1


ReturnCode ret = driver.rfalTransceiveBlockingTxRx(authCmd, sizeof(authCmd), response, sizeof(response), &responseLen, RFAL_TXRX_FLAGS_DEFAULT, RFAL_FWT_NONE);

if (ret == ERR_NONE && responseLen == 4)
{
Serial.printf("Authentication Step 1: Nonce Received %02X %02X %02X %02X\n",
response[0], response[1], response[2], response[3]);

// Here, we need to process the nonce with Crypto-1 to generate the response.
Serial.println("Crypto-1 Processing Required (Not handled by ST RFAL).");

return true;
}
else
{
Serial.printf("Authentication Failed (Step 1) %d.\n", ret);
return false;
}
}
Ulysses HERNIOSUS
Technical Moderator
March 6, 2025

Hello,

I think this 60 command is in reality much shorter. Please check against the specs of the cards in use. To my knowledge it can be sent using normal mode. First verify that. And once you get a response - as subsequent commands need to be sent in low level mode (SW generated parity and CRC)-  it will be a good idea to already exercise with this command the transmission and reception of low level frames.

A similar approach with a T2T command was discussed under keyword "template" in the mentioned other community thread.

BR, Ulysses

Visitor II
March 24, 2025

Still no progress in getting a nonce from Mifare Classic 1K.  Once I get the UID, I reverted to going directly to the registers, please see my mifare_authenticate function from which I do all the low level stuff. NOTHING.

1. Tap a tag to read its content␍␊
ISO14443A/NFC-A card found. UID: 77B2FCFF␍␊
ATQA: 04 00␊
SAK: 08␊
Detected MIFARE Classic 1K.␍␊
:locked_with_key: Starting MIFARE authentication sequence...␍␊
🧹 Resetting FIFO...␍␊
:wrench: Configuring ST25R3916 for ISO14443A...␍␊
:outbox_tray: Auth Frame: 60 04 A0 A1 A2 A3 A4 A5 FF FC B2 77 ␍␊
:inbox_tray: Writing frame to FIFO...␍␊
:satellite_antenna: Sending TRANSMIT_WITH_CRC command...␍␊
:hourglass_not_done: Waiting for IRQ response...␍␊
IRQ_MAIN: 0x7F␍␊
IRQ_ERROR: 0x7F␍␊
:white_heavy_check_mark: IRQ received: Card responded.␍␊
:package: FIFO Length: 0␊
:warning: FIFO empty, no response from card.␍␊
:incoming_envelope: Reading nonce from FIFO...␍␊
:locked_with_key: Nonce (Nt): 00 00 00 00 ␍␊
:rocket: Authentication phase 1 complete.␍␊
Operation completed␍␊
Tag can be removed from the field␍␊
1. Tap a tag to read its content␍␊
ISO14443A/NFC-A card found. UID: 77B2FCFF␍␊
ATQA: 04 00␊
SAK: 08␊
Detected MIFARE Classic 1K.␍␊
:locked_with_key: Starting MIFARE authentication sequence...␍␊
🧹 Resetting FIFO...␍␊
:wrench: Configuring ST25R3916 for ISO14443A...␍␊
:outbox_tray: Auth Frame: 60 04 A0 A1 A2 A3 A4 A5 FF FC B2 77 ␍␊
:inbox_tray: Writing frame to FIFO...␍␊
:satellite_antenna: Sending TRANSMIT_WITH_CRC command...␍␊
:hourglass_not_done: Waiting for IRQ response...␍␊
IRQ_MAIN: 0x7F␍␊
IRQ_ERROR: 0x7F␍␊
:white_heavy_check_mark: IRQ received: Card responded.␍␊
:package: FIFO Length: 0␊
:warning: FIFO empty, no response from card.␍␊
:incoming_envelope: Reading nonce from FIFO...␍␊
:locked_with_key: Nonce (Nt): 00 00 00 00 ␍␊
:rocket: Authentication phase 1 complete.␍␊
Operation completed␍␊
Tag can be removed from the field␍␊
1. Tap a tag to read its content␍␊


#define ST25R3916_REG_IO_CONF1 0x04
#define ST25R3916_REG_FIFO_LENGTH1 0x1C
#define ST25R3916_REG_FIFO_LENGTH2 0x1D
#define ST25R3916_REG_FIFO_CONTROL 0x18
#define ST25R3916_REG_FIFO_DATA 0x1F
#define ST25R3916_REG_COMMAND 0x00
#define ST25R3916_CMD_TRANSMIT_WITH_CRC 0x1A
#define ST25R3916_REG_OP_CONTROL 0x01
#define ST25R3916_REG_NFCIP1_BIT_RATE 0x08
#define ST25R3916_REG_IRQ_MAIN 0x0D
#define ST25R3916_REG_IRQ_ERROR 0x0E
#define ST25R3916_REG_FIFO_STATUS 0x1C
#define ST25R3916_REG_FIFO_LENGTH 0x1D
#define ST25R3916_REG_FIFO 0x1F
#define ST25R3916_REG_OPERATION_CONTROL 0x02
#define ST25R3916_REG_IRQ_ERROR 0x0C
#define ST25R3916_REG_IRQ_MASK_ERROR 0x17

void getTagASystemInfo(const rfalNfcDevice *device)
{
 const rfalNfcaListenDevice &nfca = device->dev.nfca;
 uint8_t atqa_0 = nfca.sensRes.anticollisionInfo;
 uint8_t atqa_1 = nfca.sensRes.platformInfo;
 uint8_t sak = nfca.selRes.sak;

 USBSerial.printf("ATQA: %02X %02X\n", atqa_0, atqa_1);
 USBSerial.printf("SAK: %02X\n", sak);

 if (atqa_0 == 0x44 && atqa_1 == 0x00 && sak == 0x00)
 {
 USBSerial.println("Detected ST25TN01K Tag!");
 }
 else if (atqa_0 == 0x04 && atqa_1 == 0x00 && sak == 0x08)
 {
 USBSerial.println("Detected MIFARE Classic 1K.");
 mifare_authenticate(0x04, device->nfcid, true);
 }
 else
 {
 USBSerial.println("Unknown NFC-A tag detected.");
 }
}

uint8_t readRegister(uint8_t regAddress)
{
 uint8_t readCommand = regAddress | 0x40; // Set the read bit

 // Prepare to send the SPI command and receive the data
 uint8_t result = 0;
 // Enable the device by pulling CS low
 digitalWrite(CS_PIN, LOW);
 // Begin the SPI transaction with 1 MHz, MSB first, and SPI mode 1
 SPI.beginTransaction(spiSettings);
 // Send the read command
 SPI.transfer(readCommand); // Send the command byte (readCommand)
 // Receive the register value
 result = SPI.transfer(0x00); // Send dummy data to clock in the register value
 // End the transaction
 SPI.endTransaction();
 // Deselect the device by pulling CS high
 digitalWrite(CS_PIN, HIGH);
 // Return the read register value
 return result;
}

void writeRegister(uint8_t regAddress, uint8_t value)
{
 uint8_t writeCommand = regAddress & 0x7F; // Clear bit 7

 digitalWrite(CS_PIN, LOW);
 SPI.beginTransaction(spiSettings);
 SPI.transfer(writeCommand); // Send register address
 SPI.transfer(value); // Send the value to write
 SPI.endTransaction();
 digitalWrite(CS_PIN, HIGH);
}
void modifyRegisterBit(uint8_t regAddress, uint8_t bitPosition, bool setBit)
{
 uint8_t value = readRegister(regAddress);

 if (setBit)
 value |= (1 << bitPosition);
 else
 value &= ~(1 << bitPosition);

 digitalWrite(CS_PIN, LOW);
 SPI.beginTransaction(spiSettings);
 SPI.transfer(regAddress & 0x7F); // Clear MSB for write
 SPI.transfer(value);
 SPI.endTransaction();
 digitalWrite(CS_PIN, HIGH);
}

void setup3v3()
{
 uint8_t regAddress = 0x01;
 modifyRegisterBit(regAddress, 7, true); // Set bit 7 to 1 for 3.3V mode
 delay(10); // Optional safety delay

 uint8_t updatedValue = readRegister(regAddress);
 USBSerial.print(":gear: 0x01 register (binary): 0b");
 for (int i = 7; i >= 0; --i)
 USBSerial.print((updatedValue >> i) & 0x01);
 USBSerial.println();
}
bool checkIrqStatus()
{
 uint8_t irqMain = readRegister(ST25R3916_REG_IRQ_MAIN);
 uint8_t irqError = readRegister(ST25R3916_REG_IRQ_ERROR);

 USBSerial.print("IRQ_MAIN: 0x");
 USBSerial.println(irqMain, HEX);
 USBSerial.print("IRQ_ERROR: 0x");
 USBSerial.println(irqError, HEX);

 if (irqMain & 0x08)
 {
 // RX IRQ — indicates a response received
 return true;
 }

 if (irqError != 0x00)
 {
 // Something went wrong
 USBSerial.println(":cross_mark: Error occurred during authentication.");
 return false;
 }

 USBSerial.println(":hourglass_not_done: No response yet...");
 return false;
}

void reset_fifo() {
 USBSerial.println("🧹 Resetting FIFO...");
 writeRegister(ST25R3916_REG_FIFO_CONTROL, 0x80);
}

void configure_mode() {
 USBSerial.println(":wrench: Configuring ST25R3916 for ISO14443A...");
 writeRegister(ST25R3916_REG_MODE, 0x00); // ISO14443A framing
 writeRegister(ST25R3916_REG_ISO14443A_NFC, 0x02); // Short frames
 writeRegister(ST25R3916_REG_OPERATION_CONTROL, 0x3C); // TX + RX
 writeRegister(ST25R3916_REG_OPERATION_CONTROL, 0x80); // RF field on
 delay(5);
}

void clear_irqs() {
 writeRegister(ST25R3916_REG_IRQ_MASK_MAIN, 0xF0);
 writeRegister(ST25R3916_REG_IRQ_MASK_ERROR, 0xFF);
 writeRegister(ST25R3916_REG_IRQ_MAIN, 0x7F);
 writeRegister(ST25R3916_REG_IRQ_ERROR, 0x7F);
}

void print_auth_frame(const uint8_t *frame, size_t len) {
 USBSerial.print(":outbox_tray: Auth Frame: ");
 for (size_t i = 0; i < len; ++i) {
 USBSerial.printf("%02X ", frame[i]);
 }
 USBSerial.println();
}

void write_auth_frame(const uint8_t *frame, size_t len) {
 USBSerial.println(":inbox_tray: Writing frame to FIFO...");
 for (size_t i = 0; i < len; ++i) {
 writeRegister(ST25R3916_REG_FIFO_DATA, frame[i]);
 }
}

bool wait_for_irq() {
 USBSerial.println(":hourglass_not_done: Waiting for IRQ response...");
 for (int i = 0; i < 10; ++i) {
 if (checkIrqStatus()) {
 USBSerial.println(":white_heavy_check_mark: IRQ received: Card responded.");
 return true;
 }
 delay(10);
 }
 USBSerial.println(":cross_mark: No IRQ detected. Authentication failed or timed out.");
 return false;
}

void read_and_print_fifo() {
 uint8_t fifoLen = readRegister(ST25R3916_REG_FIFO_LENGTH);
 USBSerial.printf(":package: FIFO Length: %d\n", fifoLen);

 if (fifoLen == 0) {
 USBSerial.println(":warning: FIFO empty, no response from card.");
 return;
 }
 if (fifoLen == 1) {
 uint8_t nak = readRegister(ST25R3916_REG_FIFO_DATA);
 USBSerial.printf(":cross_mark: NAK Byte Received: 0x%02X\n", nak);
 }

 USBSerial.print(":incoming_envelope: FIFO Data: ");
 digitalWrite(CS_PIN, LOW);
 SPI.beginTransaction(spiSettings);
 SPI.transfer(ST25R3916_REG_FIFO | 0x40);
 for (int i = 0; i < fifoLen; ++i) {
 USBSerial.printf("%02X ", SPI.transfer(0x00));
 }
 SPI.endTransaction();
 digitalWrite(CS_PIN, HIGH);
 USBSerial.println();
}

bool isFieldOn()
{
 uint8_t status = readRegister(ST25R3916_REG_OPERATION_CONTROL);
 return (status & 0x80); // Bit 7 = RF field status
}

void enableRfField()
{
 USBSerial.println(":high_voltage: Enabling RF field...");
 writeRegister(ST25R3916_REG_OPERATION_CONTROL, 0x80);
 delay(10); // Give the field some time to stabilize
}
void mifare_authenticate(uint8_t block_number, uint8_t *uid, bool use_key_a) {
 size_t short_frame_len = 2;
 size_t long_frame_len = 12;
 USBSerial.println(":locked_with_key: Starting MIFARE authentication sequence...");

 uint8_t cmd = use_key_a ? 0x60 : 0x61;
 uint8_t key[6] = {0xA0, 0xA1, 0xA2, 0xA3, 0xA4, 0xA5};
 uint8_t auth_frame[12] = {cmd, block_number};

 memcpy(&auth_frame[2], key, 6);
 auth_frame[8] = uid[3]; auth_frame[9] = uid[2];
 auth_frame[10] = uid[1]; auth_frame[11] = uid[0];

 reset_fifo();
 configure_mode();
 clear_irqs();

 size_t send_frame_len = long_frame_len;

 print_auth_frame(auth_frame, send_frame_len);
 write_auth_frame(auth_frame, send_frame_len);

 USBSerial.println(":satellite_antenna: Sending TRANSMIT_WITH_CRC command...");
 writeRegister(ST25R3916_REG_COMMAND, 0x0C);

 delay(20);

 if (!wait_for_irq()) return;

 read_and_print_fifo();

 USBSerial.println(":incoming_envelope: Reading nonce from FIFO...");
 uint8_t nonce[4] = {0};
 digitalWrite(CS_PIN, LOW);
 SPI.beginTransaction(spiSettings);
 SPI.transfer(ST25R3916_REG_FIFO | 0x40);
 for (int i = 0; i < 4; i++) {
 nonce[i] = SPI.transfer(0x00);
 }
 SPI.endTransaction();
 digitalWrite(CS_PIN, HIGH);

 USBSerial.print(":locked_with_key: Nonce (Nt): ");
 for (int i = 0; i < 4; i++) {
 USBSerial.printf("%02X ", nonce[i]);
 }
 USBSerial.println();

 USBSerial.println(":rocket: Authentication phase 1 complete.");
}

void setup()
{
 USBSerial.begin(115200);
 configureSPI();
 if (rfal_nfc.rfalNfcInitialize() == ERR_NONE)
 {
 discParam.compMode = RFAL_COMPLIANCE_MODE_NFC;
 discParam.devLimit = 1U;
 discParam.nfcfBR = RFAL_BR_212;
 discParam.ap2pBR = RFAL_BR_424;

 ST_MEMCPY(&discParam.nfcid3, NFCID3, sizeof(NFCID3));
 ST_MEMCPY(&discParam.GB, GB, sizeof(GB));
 discParam.GBLen = sizeof(GB);

 discParam.notifyCb = NULL;
 discParam.totalDuration = 1000U;
 discParam.wakeupEnabled = false;
 discParam.wakeupConfigDefault = true;
 discParam.techs2Find = (RFAL_NFC_POLL_TECH_A | RFAL_NFC_POLL_TECH_B | RFAL_NFC_POLL_TECH_F | RFAL_NFC_POLL_TECH_V | RFAL_NFC_POLL_TECH_ST25TB);
 discParam.techs2Find |= RFAL_NFC_POLL_TECH_AP2P;

 state = DEMO_ST_START_DISCOVERY;
 }
}