Skip to main content
Dalik
Associate II
November 3, 2023
Solved

NFC reader ST25R3916B EXT_LM pin

  • November 3, 2023
  • 1 reply
  • 898 views

Hi,
My application used ST25R3916B for transmit power for the card only.

1. Is it possible to leave the EXT_LM pin unused or exclude external load modulation from my application?
2. Can I use the testing point only on the pin EXT_LM pin?
Best,
Dalik LIM

 

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi Dalik,

 

not sure I completely understand: Using EXT_LM is a possibility in the chip. Technically it can work without. Foreseeing a testpoint is always a good idea.

 

Regards, Ulysses

1 reply

Ulysses HERNIOSUS
Technical Moderator
November 6, 2023

Hi Dalik,

 

not sure I completely understand: Using EXT_LM is a possibility in the chip. Technically it can work without. Foreseeing a testpoint is always a good idea.

 

Regards, Ulysses