Skip to main content
DIvan.1
Associate III
May 13, 2025
Solved

NFC10A1 on NUCLEO -F303

  • May 13, 2025
  • 2 replies
  • 734 views

Hello,

I would like to develop a system using the NFC chip ST25R200 and the microcontroller STM32F303. The main idea is to be able to read an NFC tag, specifically the ST25DV64KC.

As a first step, I plan to test this using the prototyping board NUCLEO-F303 and the NFC expansion board X-NUCLEO-NFC10A1. I'm using CubeIDE.

I'm sure that ST has prepared everything for a simple and smooth integration. Because of that, I'm confused about what I'm doing wrong.

After configuring the pins and integrating the middleware/software in STM32CubeMX, I get errors when I try to compile the code (I haven't changed anything in the generated code).

 

Here is picture with Pins defined:

image.png

here is Middleware/software package included and set:

image.png  image.png

SPI1, Interrupt, GPIO configure:

image.pngimage.pngimage.png 

 

 

After generating code I go to main.c where I want to compile generated code and get a lot of errors:

image.png

image.png

Can you please help me understand what I'm doing wrong?
In the past, I worked with the ST25R3912, so I have some experience.
If you need more information, feel free to ask.

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

make sure to select an RFAL configuration. It seems not selected in your case:

BrianTIDAL_0-1747139936791.png

This should be something like:

BrianTIDAL_1-1747139993909.png

See attached ioc file as an example.

Rgds

BT

2 replies

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
May 13, 2025

Hi,

make sure to select an RFAL configuration. It seems not selected in your case:

BrianTIDAL_0-1747139936791.png

This should be something like:

BrianTIDAL_1-1747139993909.png

See attached ioc file as an example.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DIvan.1
DIvan.1Author
Associate III
May 13, 2025

That solved my problem.

Thank you very much.

If I want to use NFC-V and allowed energy harvesting for tag (ST25DV64KC)...

1. what is the minimum of the functions I need to use?

2. what of these options I need to use:

image.pngimage.png

 

I'm a bit sceptical with time spending using all that functions.

 

Thank you and best regards,

 

Brian TIDAL
Technical Moderator
May 13, 2025

Hi,

in a perfect world, you should choose Custom_config for the RFAL and then select RFAL_FEATURE_NFCV and RFAL_FEATURE_ST25xV and regenerate. In that case the project also defines RFAL_ANALOG_CONFIG_CUSTOM whereas no custom analog config are provided, so #define RFAL_ANALOG_CONFIG_CUSTOM needs to be manually commented in the nfc_conf.h.

Unselected technologies are then not used in the discovery loop and the linker removes the unused part of the code. 

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Brian TIDAL
Technical Moderator
May 14, 2025

Hi,

Sorry for the confusion about RFAL_ANALOG_CONFIG_CUSTOM, I was using a pre-release version of the FW package.

Regarding RAM/FLASH usage

Default:

BrianTIDAL_0-1747227903785.png

Custom:

BrianTIDAL_1-1747227957648.png

Make sure to use the following compiler settings:

BrianTIDAL_2-1747228173313.png

and the following linker setting:

BrianTIDAL_3-1747228202219.png

Check the map file for the custom build vs the default build: functions such as rfalNfcaPollerInitialize should be absent in the custom build map file.

Also adjust the compiler optimization level according to your needs.

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.