Associate II
February 14, 2025
Solved
Peer to Peer Communications between ST25R3916B and ST25R3918
- February 14, 2025
- 6 replies
- 1998 views
I have two Nucleo boards, both NUCLEO-L476RG. The first board is equipped with the X-NUCLEO-NFC08A1 (ST25R3916B), while the second board has the NFC 5 Click board (ST25R3918).
I am trying to establish peer-to-peer (P2P) communication between these boards, with the ST25R3916B configured as the initiator and the ST25R3918 as the target.
Both boards successfully detect NFC tags, confirming that the basic hardware setup is functioning correctly. However, I have not been able to achieve P2P communication.
Any guidance or assistance in resolving this issue would be greatly appreciated. I have attached the initiator and target codes for reference.