Skip to main content
Jhern.1
Associate III
February 10, 2022
Solved

Reading emulated cards with St25r95 / St95hf

  • February 10, 2022
  • 6 replies
  • 2182 views

Hello,

I am trying to read data from iOS/Andriod App with my reader.

Currently, my reader is based on st25r95 and it is in tag detector mode waiting for physical cards. Everthing is ok so far. Now I need to wakeup and get data from smartphone or pshysical card.

For getting data from iOs/Android App I guess I have 2 options:

  • Use HCE in smartphone and read the data as a physical tag. But not sure if ST25R95 supports this or I need to meve to st95Hf, or which protocol to use, methods, etc.
  • Use P2P, but I think p2p is only supported in ST95HF.

My preferred choice is to go with HCE, but not sure how to proceed.

Can you confirm this can be done with st25r95?

I think I have to use 14443A protocol, but not sure if I need an upper FW layer for handlng this.

I can not find any app in playstore to emulate tags. Can you provide any recommendation on how to test this.

Regards, Ramon.

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi Ramon,

    an NDEF stack is provided on top of the RFAL. An NDEF read/write demo application is available in the ST25 Embedded NFC library for X-NUCLEO-NFC03A1 (ST25R95 expansion board). I would recommend to use this demo for your application as this provides all you need for NDEF read/write with the proper RFAL configuration.

    Regarding your Android App, I see in the trace that the answer to NDEF Application select is incorrect (<<< 8007F2019140080000). Can you make sure the NDEF Android App is currently running in foreground? There should be no popup on the phone when it receives the NDEF Application Select APDU. Which phone (brand/model) do you use? Which NDEF App do you use?

    Rgds

    BT

    6 replies

    Brian TIDAL
    Technical Moderator
    February 10, 2022

    Hi Ramon,

    A device in Card Emulation mode acts as a physical tag. Therefore, you can directly use the ST25R95 reader to communicate with the Emulated Card and to read its content.

    Usually, Android phones emulates T4AT and/or T3T tags.

    Regarding Active Peer To Peer (AP2P), this is supported by ST25R3916 device but not supported by ST25R95 nor ST95HF. Be aware that not all NFC-enabled Android phones are supporting NFC P2P anymore. With Android 10 Google has marked the APIs as deprecated (https://developer.android.com/guide/topics/connectivity/nfc/nfc#p2p). Android Beam is disappearing.

    Regarding ST95HF and ST25R95: both can act as reader but also can act as an Emulated Card (this is the meaning of Card Emulation feature being supported by those devices). When acting as a reader, both ST95HF and ST25R95 can communicate with a device acting in Card Emulation mode.

    In the play store, you can search for something like NFC NDEF emulation.

    Feel free to provide more information about your use case.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Jhern.1
    Jhern.1Author
    Associate III
    February 10, 2022

    OK,

    Thanks for answering so quick.

    That´s what I thought, but I wanted it to confirm it.

    I am using NDEF tag emulator in my Andriod phone. But I Can not read a simple NDEF message with my evaluation kit (NDEF type 4A).

    0693W00000JPHj4QAH.png 

    When clicking "READ NDEF MESSAGE" a list of service pops up on the phone, I select the one for the emulator and nothing more happens.

    0693W00000JPHjAQAX.pngFull log:

    02-10-2022 12:07:18	RESET SPI
    			>>> CR95HFDll_RESETSPI
    			<<< 8000
    02-10-2022 12:07:18	ECHO
    			>>> CR95HFDll_ECHO
    			<<< 5500
    02-10-2022 12:07:18	RF OFF
    02-10-2022 12:07:18	CR95HF CONFIGURATION : ISO14443-A protocol
    			>>> CR95HFDLL_SELECT, 02000280
    			<<< 0000
    02-10-2022 12:07:18	ISO14443-A : CONFIG
    			>>> CR95HFDLL_STCMD, 0109043A005804
    			<<< 0000
    02-10-2022 12:07:18	ISO14443-A : INCREASE DEMOD GAIN
    			>>> CR95HFDLL_STCMD, 010904680101D3
    			<<< 0000
    02-10-2022 12:07:18	RF ON
    02-10-2022 12:07:18	ISO14443A REQ-A
    			>>> CR95HFDLL_SENDRECEIVE, 2607
    			<<< 0400
    02-10-2022 12:07:18	ISO14443A ANTICOL 1
    			>>> CR95HFDLL_SENDRECEIVE, 932008
    			<<< 08869A7C68
    02-10-2022 12:07:18	ISO14443A SELECT 1
    			>>> CR95HFDLL_SENDRECEIVE, 937008869A7C6828
    			<<< 20FC70
    02-10-2022 12:07:18	ISO14443-A RATS
    			>>> CR95HFDLL_SENDRECEIVE, E04028
    			<<< 05788071006F7C
    02-10-2022 12:07:18	ISO14443-A PPS
    			>>> CR95HFDLL_SENDRECEIVE, D0110028
    			<<< D07387
    02-10-2022 12:07:18	TAG DETECTED (UID = 08869A7C)
     
    02-10-2022 12:07:18	NFC SEND I-Block - Select Appli
    			>>> CR95HFDLL_SENDRECEIVE, 0200A4040007D27600008501010028
    			<<< 8007F2019140080000
    02-10-2022 12:07:18	!!! NO ANSWER DURING RF COMMUNICATION

    Any guess about what is happening?

    What about the emulated cards in iOS? Which type I need to use to read the NDEF?

    Regards, Ramon.

    Jhern.1
    Jhern.1Author
    Associate III
    February 10, 2022

    One more thing. In terms of RFAL, which would be the stack to use:

    0693W00000JPI3oQAH.png 

    T4T and ISODEP?

    Regards, Ramon.

    Brian TIDAL
    Brian TIDALBest answer
    Technical Moderator
    February 10, 2022

    Hi Ramon,

    an NDEF stack is provided on top of the RFAL. An NDEF read/write demo application is available in the ST25 Embedded NFC library for X-NUCLEO-NFC03A1 (ST25R95 expansion board). I would recommend to use this demo for your application as this provides all you need for NDEF read/write with the proper RFAL configuration.

    Regarding your Android App, I see in the trace that the answer to NDEF Application select is incorrect (<<< 8007F2019140080000). Can you make sure the NDEF Android App is currently running in foreground? There should be no popup on the phone when it receives the NDEF Application Select APDU. Which phone (brand/model) do you use? Which NDEF App do you use?

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Jhern.1
    Jhern.1Author
    Associate III
    February 10, 2022

    App: "NDEF Tag emulator"

    Phone: Huawei P20 Lite

    Android: 9.1.0

    Yes, app is running foreground and saying "Emulating...."

    0693W00000JPJHqQAP.pngPopUp arises as there are several compatible services (My guess)

    0693W00000JPJHCQA5.pngNFC Service is the logo of the App NFC Tag emulator

    Brian TIDAL
    Technical Moderator
    February 10, 2022

    Hi,

    I used to have the same popup on my personal Android phone:

    go to the parameters/settings menu in Android, then NFC payement & contactless then contactless payement then Others and deselect all except NdefTagEmulator.

    The popup should not appears any longer and the NDEF can be read

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.