Skip to main content
KVoul.1
Associate II
September 1, 2021
Solved

Rewire IRQ pin in NUCLEO-NFC06A1

  • September 1, 2021
  • 1 reply
  • 710 views

Hello, I accidentally connected Vcc to the interrupt pin in an X-NUCLEO-NFC06A1, now I don't get any interrupts. Is it terminally burnt or can I configure an IRQ from somewhere else on the board?

This topic has been closed for replies.
Best answer by Peter BENSCH

The interrupt pin of the X-NUCLEO-NFC06A1 is connected to pin IRQ of the ST25R3916, which is an output, most likely destroyed and no chance to get the IRQ from somewhere else.

The only possibilities: replace the ST25R3916 or get a new X-NUCLEO-NFC06A1.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
September 1, 2021

The interrupt pin of the X-NUCLEO-NFC06A1 is connected to pin IRQ of the ST25R3916, which is an output, most likely destroyed and no chance to get the IRQ from somewhere else.

The only possibilities: replace the ST25R3916 or get a new X-NUCLEO-NFC06A1.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter