Skip to main content
OliM
Senior
August 5, 2022
Solved

Right way to ignore received CRC in ST25R3916 with RFAL

  • August 5, 2022
  • 4 replies
  • 1108 views

I am expecting an answer from an ISO14443-2 Tag with no CRC set, so I want to disable that check. Currently I am doing a rfalTransceive with the following flags

( (uint32_t)RFAL_TXRX_FLAGS_CRC_TX_AUTO | (uint32_t)RFAL_TXRX_FLAGS_NFCIP1_OFF | (uint32_t)RFAL_TXRX_FLAGS_AGC_ON | (uint32_t)RFAL_TXRX_FLAGS_PAR_TX_AUTO | (uint32_t)RFAL_TXRX_FLAGS_NFCV_FLAG_AUTO \

            | (uint32_t)RFAL_TXRX_FLAGS_CRC_RX_MANUAL | (uint32_t)RFAL_TXRX_FLAGS_CRC_RX_KEEP | (uint32_t)RFAL_TXRX_FLAGS_PAR_RX_REMV)

As a result I get a return value of ERR_CRC but also the expected length and data inside my provided response Memory. Is this expected behavior and I should just ignore the error code or is there a different flag I should use?

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi,

the mentioned NULL deref bug has been identified already and will be fixed in the next version. I think on our used test platform NULL/0 was a legitimate address.

If you find issues, you can either report them here or go through your contacts into ST sales representatives.

Best Regards, Ulysses

4 replies

Ulysses HERNIOSUS
Technical Moderator
August 8, 2022

Hi,

not sure, no ERR_CRC should be triggered. Which RFAL version are you using, which demo board and could you share some more of your demo code, not just the flags?

Best Regards, Ulysses

OliM
OliMAuthor
Senior
August 9, 2022

Hi,

I am using an X-NUCELAO-NFC06A1 on an STM32L562E-DK with RFAL version 2.6.0. After an NFC-A target without ISO-DEP support was detected i run the following code:

#define NO_RX_CRC_FLAGS ( (uint32_t)RFAL_TXRX_FLAGS_CRC_TX_AUTO | (uint32_t)RFAL_TXRX_FLAGS_NFCIP1_OFF | (uint32_t)RFAL_TXRX_FLAGS_AGC_ON | (uint32_t)RFAL_TXRX_FLAGS_PAR_TX_AUTO \
 | (uint32_t)RFAL_TXRX_FLAGS_CRC_RX_MANUAL | (uint32_t)RFAL_TXRX_FLAGS_CRC_RX_KEEP | (uint32_t)RFAL_TXRX_FLAGS_PAR_RX_REMV )
...
const uint8_t AuthKeyA[] = {0x60, 0x00};
uint8_t RxBuff[255] = {0};
uint16_t RcvLen = 0;
Err = rfalTransceiveBlockingTxRx((uint8_t*)AuthKeyA, sizeof(AuthKeyA), (uint8_t*)RxBuff, sizeof(RxBuff), &RcvLen, MFC_NO_RX_CRC_FLAGS, RFAL_1MS_IN_1FC);

As you might have guessed by now I will also have to do parity by hand afterwards, but I still don't get why there is an error message for the answer here.

Ulysses HERNIOSUS
Technical Moderator
August 9, 2022

Hi,

I have experience with RFAL_TXRX_FLAGS_PAR_RX_KEEP instead of RFAL_TXRX_FLAGS_PAR_RX_REMV. In that scenario no ERR_CRC gets signaled.

Could you do logic analyzer traces and check the value of the register 0x0a (Auxiliary Definition register).

Best Regards, Ulysses

OliM
OliMAuthor
Senior
August 9, 2022

I get the same ERR_CRC no matter whether I use RFAL_TXRX_FLAGS_PAR_RX_KEEP or RFAL_TXRX_FLAGS_PAR_RX_REMV.

I have no logic analyzer connected at the moment so all I could offer for register states are debug points inside RFAL.

Ulysses HERNIOSUS
Technical Moderator
August 9, 2022

Hi,

A logic analyzer trace will help so much more as there is also a possibility of looking at a porting artifact.

BR, Ulysses

OliM
OliMAuthor
Senior
August 9, 2022

I have to admit that it's not a priority for me right now since I can read both ISO and non ISO cards (MFC) completely and only get that return value in the specific case where I want to ignore CRC on receive but still generate the send CRC and parity by hardware.

On another note: What's the best place to report bugs in RFAL?

This one is quite obvious:

ReturnCode rfalWakeUpModeStart( const rfalWakeUpConfig *config )
{
 uint8_t aux;
 uint8_t reg;
 uint32_t irqs;
 
 /* Check if RFAL is not initialized */
 if( gRFAL.state < RFAL_STATE_INIT )
 {
 return ERR_WRONG_STATE;
 }
 
#ifdef ST25R3916B
 /* Check for not supported features */
 if( config->cap.enabled )
 {
 return ERR_NOTSUPP;
 }
 
 /* Set ST25R3916B Measure Tx delay */
 st25r3916WriteRegister(ST25R3916_REG_MEAS_TX_DELAY, ( st25r3916IsAATOn() ? RFAL_ST25R3916B_AAT_SETTLE : 0x00) );
#endif /* ST25R3916B */
 
 /* The Wake-Up procedure is explained in detail in Application Note: AN5320 */
 
 if( config == NULL )
 {
 gRFAL.wum.cfg.period = RFAL_WUM_PERIOD_200MS;
 gRFAL.wum.cfg.irqTout = false;

line15 accesses NULL when default config is selected on upper level.

That was the first thing I encountered when switching to ST25R3916B (on a self modified NFC06A1 board), but the CRC behavior remains the same as before.