Skip to main content
LePluc
Associate
October 20, 2022
Solved

shield-m24sr-adv

  • October 20, 2022
  • 2 replies
  • 1544 views

Hi,

I've got a x-nucleo board marked shield-m24sr-adv and I'm unable to find any docs about it. Well of course its a NFC reader board but.......

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome, @LePluc​, to the community!

Unfortunately, there is officially no more information about the SHIELD-M24SR-ADV, since it only existed for a short time. It was then replaced by the very similar successor X-NUCLEO-NFC01A1, which is based on the same NFC chip M24SR64-YMN6T/2.

Regards

/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
October 20, 2022

Welcome, @LePluc​, to the community!

Unfortunately, there is officially no more information about the SHIELD-M24SR-ADV, since it only existed for a short time. It was then replaced by the very similar successor X-NUCLEO-NFC01A1, which is based on the same NFC chip M24SR64-YMN6T/2.

Regards

/Peter

LePluc
LePlucAuthor
Associate
October 20, 2022

Thanks for the swift answer!

Ulysses HERNIOSUS
Technical Moderator
October 20, 2022

Hi,

I think this is rather a tag board than a reader board which seems to have been discontinued quite some years ago.

From a quick glimpse it seems very similar to x-nucleo-nfc01a1 which I would use instead because for it you find all kinds of support material.

Best Regards, Ulysses

LePluc
LePlucAuthor
Associate
October 20, 2022

Thanks for the swift answer, obsolete...well I guess that's what you get when store stuff in the wrong box :)