Skip to main content
PBuro.1
Associate II
May 31, 2023
Solved

Some questions regarding reader handling with the ST25SDK

  • May 31, 2023
  • 1 reply
  • 1020 views

Hi,

So I'm using the ST25SDK to create an app. I managed to detect my USB Reader and detect tags from it. But I am wondering if there is a way to chose which reader to use if several are connected by USB.

Also, I cannot find a way to connect to an ethernet reader. The demo app (ST25PC002) there seems to be that possibility, but only using a ST Reader, not Feig (the only readers I have underhand are Feig MR101 USB and ethernet). And it seems to use a JNI interface and a specific implementation of RFGenericReader that overload the connect method to add the IP as a parameter. I cannot find any reference to that overloaded method in the SDK javadoc. Does the SDK handle ethernet reader easily ? for either ST or Feig readers ?

Thank you for your help

    This topic has been closed for replies.
    Best answer by Damien G.

    Hello,

    you can find an example of reader handling in the source code of the ST25PC-NFC software as you already have mentioned.
    Check out code from function scanForReaders() in MainApp.java. There we try to instantiate a STReader object. If we fail, we then try to instantiate a FEIG_OBID_ISC_Reader. Today we do not select a specific reader based on its port number as we only handle one reader at a time.

    You are correct, the ST25SDK only handles Ethernet connection for an internal ST reader through a JNI. If you want to connect to a FEIG reader using Ethernet instead of USB, you should take a look at the FEIG OBID SDK available from the FEIG ELECTRONIC website.

     

    Best regards,
    Damien

    1 reply

    Damien G.Best answer
    ST Employee
    June 19, 2023

    Hello,

    you can find an example of reader handling in the source code of the ST25PC-NFC software as you already have mentioned.
    Check out code from function scanForReaders() in MainApp.java. There we try to instantiate a STReader object. If we fail, we then try to instantiate a FEIG_OBID_ISC_Reader. Today we do not select a specific reader based on its port number as we only handle one reader at a time.

    You are correct, the ST25SDK only handles Ethernet connection for an internal ST reader through a JNI. If you want to connect to a FEIG reader using Ethernet instead of USB, you should take a look at the FEIG OBID SDK available from the FEIG ELECTRONIC website.

     

    Best regards,
    Damien