Skip to main content
NKern.1
Associate II
January 21, 2022
Solved

ST25DV_Discovery_ANT_C6 is working, but C1 is not.

  • January 21, 2022
  • 5 replies
  • 5617 views

Nordic board + ST25DV_Discovery_ANT_C6 = works great.

Nordic board + ST25DV_Discovery_ANT_C1 = does NOT work (ST25 is not recognized).

Why?

What is the operational difference between C6 and C1?

This topic has been closed for replies.
Best answer by NKern.1

On another setup it somehow worked properly without modifications.

Appreciate your advises.

5 replies

Ulysses HERNIOSUS
Technical Moderator
January 21, 2022

Hi NKern.1,

could you detail a bit more on the reader side and its antenna size?

Best Regards, Ulysses

NKern.1
NKern.1Author
Associate II
January 21, 2022

C6 has small antenna.

C1 has large antenna.

Connected via I2C to Nordic nRF52-DK.

Connection is identical in both cases, but with C1 Nordic fails to initialize the ST25.

Ulysses HERNIOSUS
Technical Moderator
January 24, 2022

Hi,

ah, I think I was mistaken - I thought the NFC communication is not working due to antenna size. But you mean with the board with the C1 antenna nRF52-DK cannot access the ST25DV via I2C?!

Ulysses

JL. Lebon
ST Employee
January 28, 2022

Hello,

On I2C side, the ST25DV_Discovery_ANT_C1 and the ST25DV_Discovery_ANT_C6 are identical. The only differences between the two boards is the size of the antennas.

So in theory, if you can access the C6, you should also be able to access the C1 in the exact same way.

You can check on ST25DV_Discovery_ANT_C1 that R2 and R3 are correctly populated: those are the pull-ups for the I2C signals.

You can also check ST1 jumper: it should connect 1 and 2 for the VCC to be connected to 3v3. If pin 2 and 3 are connected instead, the VCC of St25DV is coming from energy harvesting, which is probably not what you want.

Please also note that on some boards (C1 as well as C6), R1 is wrongly populated. You can remove it for correct GPO behavior. But this should not cause an issue with I2C.

Best regards.

NKern.1
NKern.1AuthorBest answer
Associate II
February 8, 2022

On another setup it somehow worked properly without modifications.

Appreciate your advises.

JL. Lebon
ST Employee
February 8, 2022

Hello,

What do you mean by "other setup" ? Can you be more precise ?

Did you check the R2 and R3 resistors and ST1 jumper as suggested ?

For reasons I don't know the schematics of those boards is not available on the st.com web site, so I have attached them here for you to be able to check.

Best regards.

JL. Lebon
ST Employee
February 8, 2022