Skip to main content
Associate
October 6, 2025
Solved

ST25DVCryptoDemo iOS not working

  • October 6, 2025
  • 25 replies
  • 1738 views

Hello @all,

 

I've downloaded ST25DVCryptoDemo for iOS from here, in order to take a look into the demo code for a new project.
Once I've tried to build the Demo app I've got a big amount of errors. In fact the console gave me this message "too many errors emitted, stopping now"


Screenshot 2025-10-06 at 12.16.17.png

Could someone please help me to fix those issues and make everything works properly?
I've also download the ST25SDK but, when I've took a look the Readme file I saw that the SDK can be used for Android app and PC app (not iOS app)

Best answer by victor laraison

Hi ,

Regarding your questions, ST’s iOS app does not require any private Apple entitlement to enable or use the FTM mailbox of the ST25DV. The only entitlement needed for all our iOS NFC applications is the standard iOS coreNFC entitlement.

If you review the source code of the iOS NFC Tap application (refer to STSW-ST25IOS001 | Product - STMicroelectronics), you will find numerous examples demonstrating how to use the FTM mailbox.

Specifically, you can refer to ST25DVI2CDataTransfertViewController.swift for the UI implementation and the folder \st25sdklib\include\com\st\st25sdk\ftmprotocol for the FTM protocol used in our demo.

Another important point to note is that iOS CoreNFC custom commands operate only in non-addressed mode, and the manufacturer code is automatically appended by the iOS custom command itself.
I let you have a look into a previous support here : Solved: NFC - ST25DV - How to use custom commands in my ow... - STMicroelectronics Community

If you need further support or assistance, please feel free to reach out.



25 replies

victor laraison
ST Employee
October 6, 2025

Hi,

Our ST25DVCryptoDemo iOS application utilizes J2ObjC, an open-source tool developed by Google, to enable cross-platform code sharing between Android and iOS.

For more details on the compilation process, please refer to an earlier ticket addressing this topic:

Solved: Error while compiling latest IOS NFC source code - STMicroelectronics Community

Hope it helps.
Br,

 

Andrea123Author
Associate
October 7, 2025

I've tried to do all the instructions that you posted in the other comment.
But it's not working.

I tried both for ST25DVCryptoDemo (version 1.0 build 1.0) and NFCTap (version 23.0 build 1.0).

I've downloaded the master version of J2ObjC.

Once the "make dist" finished to run I've copied and pasted the directory into ST25DVCryptoDemo and NFCTap.

Linked the references of j2ObjC in Build Settings.

Run clean and the build, but it's not working

Screenshot 2025-10-07 at 12.24.59.pngScreenshot 2025-10-07 at 12.26.28.png

victor laraison
ST Employee
October 7, 2025

Hi,

Depending on your environment, the compilation issues could be caused by the following:

  • The header search paths in your build settings might not be in the correct order. Please verify them against my environment, as shown in the attached screenshot.
  • The versions used on st.com rely on J2OBJ version 2.4. The latest version and master branch introduced compatibility breaks with our ST25SDK iOS Objective-C source code.

I recommend switching to version 2.4. If that is not possible, I can provide patches to support the latest J2OBJ version.

Hope it helps. Let us know.

 

Andrea123Author
Associate
October 8, 2025

@victor laraison 

I've tried to clone j2objc 2.4, but I'm not able to run the command make dist.
Here is the make dist command error:

degaspaa@WMCVSPD005 ~ % cd j2objc 
degaspaa@WMCVSPD005 j2objc % git status
HEAD detached at 2.4
nothing to commit, working tree clean
degaspaa@WMCVSPD005 j2objc % make dist
Locale:
Darwin WMCVSPD005.local 24.6.0 Darwin Kernel Version 24.6.0: Mon Jul 14 11:30:55 PDT 2025; root:xnu-11417.140.69~1/RELEASE_ARM64_T6031 arm64
Xcode 16.4 Build version 16F6
Apple clang version 17.0.0 (clang-1700.0.13.5)
Target: arm64-apple-darwin24.6.0
Thread model: posix
InstalledDir: /Applications/Xcode.app/Contents/Developer/Toolchains/XcodeDefault.xctoolchain/usr/bin

Environment:
HOME=/Users/degaspaa
HOMEBREW_CELLAR=/opt/homebrew/Cellar
HOMEBREW_PREFIX=/opt/homebrew
HOMEBREW_REPOSITORY=/opt/homebrew
INFOPATH=/opt/homebrew/share/info:
JAVA_HOME=/opt/homebrew/Cellar/openjdk@11/11.0.28/libexec/openjdk.jdk/Contents/Home
LC_CTYPE=UTF-8
LOGNAME=degaspaa
MAKEFLAGS=
MAKELEVEL=1
MANPATH=/Applications/Xcode.app/Contents/Developer/Platforms/MacOSX.platform/Developer/SDKs/MacOSX.sdk/usr/share/man:/Applications/Xcode.app/Contents/Developer/Platforms/MacOSX.platform/usr/share/man:/Applications/Xcode.app/Contents/Developer/usr/share/man:/Applications/Xcode.app/Contents/Developer/Toolchains/XcodeDefault.xctoolchain/usr/share/man:
MFLAGS=
PATH=/Users/degaspaa/.pyenv/shims:/Users/degaspaa/.pyenv/bin:/opt/homebrew/Cellar/openjdk@11/11.0.28/libexec/openjdk.jdk/Contents/Home/bin:/opt/homebrew/lib/ruby/gems/3.3.0/bin:/opt/homebrew/opt/ruby/bin:/Users/degaspaa/.sdkman/candidates/java/current/bin:/opt/homebrew/bin:/opt/homebrew/sbin:/usr/local/bin:/System/Cryptexes/App/usr/bin:/usr/bin:/bin:/usr/sbin:/sbin:/var/run/com.apple.security.cryptexd/codex.system/bootstrap/usr/local/bin:/var/run/com.apple.security.cryptexd/codex.system/bootstrap/usr/bin:/var/run/com.apple.security.cryptexd/codex.system/bootstrap/usr/appleinternal/bin:/Library/Apple/usr/bin:/Users/degaspaa/.gem/bin:/Users/degaspaa/Development/flutter/bin:/Users/degaspaa/.rvm/bin
PWD=/Users/degaspaa/j2objc
PYENV_ROOT=/Users/degaspaa/.pyenv
PYENV_SHELL=zsh
SDKMAN_CANDIDATES_API=https://api.sdkman.io/2
SDKMAN_CANDIDATES_DIR=/Users/degaspaa/.sdkman/candidates
SDKMAN_DIR=/Users/degaspaa/.sdkman
SDKMAN_PLATFORM=darwinarm64
SHELL=/bin/zsh
SHLVL=2
SSH_AUTH_SOCK=/private/tmp/com.apple.launchd.kPUAgvAbGX/Listeners
TERM=xterm-256color
TERM_PROGRAM=Apple_Terminal
TERM_PROGRAM_VERSION=455.1
TERM_SESSION_ID=7DEC8B74-4A9A-4F53-833B-C6E9754286BB
TMPDIR=/var/folders/8c/5k5986jj10ngnmmbgb_hkrr80000gn/T/
USER=degaspaa
XPC_FLAGS=0x0
XPC_SERVICE_NAME=0
rvm_alias_expanded=
rvm_bin_flag=
rvm_bin_path=/Users/degaspaa/.rvm/bin
rvm_docs_type=
rvm_gemstone_package_file=
rvm_gemstone_url=
rvm_hook=
rvm_niceness=
rvm_nightly_flag=
rvm_only_path_flag=
rvm_path=/Users/degaspaa/.rvm
rvm_prefix=/Users/degaspaa
rvm_pretty_print_flag=
rvm_proxy=
rvm_quiet_flag=
rvm_ruby_bits=
rvm_ruby_file=
rvm_ruby_make=
rvm_ruby_make_install=
rvm_ruby_mode=
rvm_script_name=
rvm_sdk=
rvm_silent_flag=
rvm_use_flag=
rvm_version=1.29.12 (latest)

mvn -q generate-resources dependency:sources
make[1]: *** [/Users/degaspaa/j2objc/java_deps/build_result/.maven_generate] Error 6
make: *** [java_deps_dist] Error 2

 

Here is some extra info:

Xcode 16.4 - Build version 16F6
MAC - 
Apple M3 Max
macOS - Version 15.6.1 (24G90)

Andrea123Author
Associate
October 13, 2025

@victor laraison 

can you please help me?
I'm not able to run the command make dist on j2objc version 2.4

victor laraison
ST Employee
October 13, 2025

Please, could you provide us more error log ? previous log was unclear for me.
Thx and br,

 

Andrea123Author
Associate
October 13, 2025

I've run git clone https://github.com/google/j2objc.git in order to download J2ObjC

Then I moved into j2objc folder and run git checkout 2.4 in order to get the 2.4 tag.

Then I run make dist and I got this error:

 

make[1]: *** [/Users/degaspaa/j2objc/java_deps/build_result/.maven_generate] Error 6
make: *** [java_deps_dist] Error 2

 

victor laraison
ST Employee
October 13, 2025

This usually means a problem running Maven commands or downloading/building Java dependencies.

1) Make sure you have Apache Maven installed and it is accessible from your command line.
bash
mvn -v
J2ObjC requires Maven 3.x 

2. Check Java JDK installation and version
J2ObjC requires a JDK (not just JRE). Verify your Java version:

bash
java -version
javac -version
Ensure you have JDK 8 or higher installed.
If you have multiple Java versions, ensure the JAVA_HOME environment variable points to the correct JDK.

3. Check network and proxy settings
If Maven fails to download dependencies, it could be due to network issues or proxy settings.

Ensure you have internet access.
If behind a proxy, configure Maven proxy settings in ~/.m2/settings.xml.

 

Hope it helps

 

victor laraison
ST Employee
October 14, 2025

for  your need, I have uploaded on iCloud shared drive a binary version of J2OBJC V2.4 used within my  environment. You can download then try it with the link 

https://www.icloud.com/iclouddrive/097v0LGJypd822A2Mtx7sHeuA#j2objc-2.4

hope it helps

Br,

Visitor II
October 17, 2025

Hi,

I'm a colleague of Andrea123. I followed the same procedures as him to install Apache Maven (3.9.11), Java (11), and I'm also using version 2.4 of J2ObjC. We both encounter the following error:

/Users/luca/Documents/STSW-ST25IOS002/NFCTap/st25sdklib/include/com/st/st25sdk/STException.h:27:10: fatal error: 'java/lang/Throwable.h' file not found.

We have insert into the Xcode the correct path for the j2objc folder: J2OBJC_HOME = $(PROJECT_DIR)/Frameworks/j2objc-2.4

 

victor laraison
ST Employee
October 17, 2025

Hi Luca,

The error 'java/lang/Throwable.h' file not found typically indicates an issue with the header search path.

Please verify your header search path settings and ensure that the J2OBJC_HOME variable is set to $(PROJECT_DIR)/Frameworks/j2objc-2.4/ with a trailing slash (/) at the end.

I hope this helps.

Visitor II
October 17, 2025

Screenshot 2025-10-17 alle 16.29.53.pngScreenshot 2025-10-17 alle 16.30.01.pngThis is the path with the fix. But the problem is still present.

Visitor II
October 21, 2025

Hi,

I insert the correct path, but now the out is like into the attachment.

Do you have any idea? in particular are you sure that this SDK works with iOS 26 and the last Xcode version?

Thanks