Skip to main content
WGorm.1
Associate
September 21, 2022
Solved

ST25R reader for MB89R118C tag

  • September 21, 2022
  • 3 replies
  • 1078 views

Which ST25R reader would you recommend for the MB89R118C Fujitsu Tag which has FRAM of 256 memory blocks/ 2048 bytes and uses ISO/IEC15693? For some reasons I could not write or read from this NFC type 5 tag with the NFC Tap app? Please advise.

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi,

    MB89R118C is a 8-byte per block device. This can be read by any of the ST25R device (ST25R95, ST25R3911B or ST25R3916/3916B).

    In ISO/IEC15693 mode, NFC Tap app is limited to 4-byte per block device thus MB89R118C cannot be read by this app.

    Rgds

    BT

    3 replies

    Brian TIDAL
    Brian TIDALBest answer
    Technical Moderator
    September 21, 2022

    Hi,

    MB89R118C is a 8-byte per block device. This can be read by any of the ST25R device (ST25R95, ST25R3911B or ST25R3916/3916B).

    In ISO/IEC15693 mode, NFC Tap app is limited to 4-byte per block device thus MB89R118C cannot be read by this app.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    WGorm.1
    WGorm.1Author
    Associate
    September 21, 2022

    Thank you so much! Would you recommend another app that may do 8-byte per block if any?

    Brian TIDAL
    Technical Moderator
    September 21, 2022

    Well, difficult for me to recommend an app from the competition ;) but if you google "app NFC Tag Info", you should find some apps.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.