Skip to main content
ANaud.1
Associate III
May 7, 2021
Solved

ST25R3916 or 3917 with two antenna

  • May 7, 2021
  • 2 replies
  • 952 views

Hi,

I was wondering if we can use the ST25R3916 or 3917 with two antenna. We connect one on the output/input of the RFO1/RFI1 and the other on the RF02/RFI2. Is that something possible ? I can't seem to find my answer in the datasheet.

Also, I want to know what is the major difference between 3916 and 3917, as they have the same datasheet.

Thanks !

This topic has been closed for replies.
Best answer by Travis Palmer

Hello ANaud.1,

please have also a look at AN5592 - "ST25R single ended antenna matching" appnote.

It could provide additional information about this topic.

Using the bit "rfo2" (Figure 12 of the mentioned application note) you could select between the two antennas.

br Travis

2 replies

Ulysses HERNIOSUS
Technical Moderator
May 10, 2021

H ANaud.1

please see table 1 of the datasheet for the differences between 3916 and 3917 (17 has no AAT, Card-Emulation and capacitive sensor).

For a bigger picture you may want to see also the slide 4 of ST25R3916_product_presentation-v1.0-Feb2019.pdf.

Yes it is possible to connect two antennas. Please see e.g. https://community.st.com/s/question/0D50X00009bLV0iSAG/st25r3911b-with-two-antenna-in-single-ended-mode which talks about this possibility on ST25R3911B. But the concept and the bits are identical.

Best Regards, Ulysses

Travis Palmer
Travis PalmerBest answer
ST Employee
May 10, 2021

Hello ANaud.1,

please have also a look at AN5592 - "ST25R single ended antenna matching" appnote.

It could provide additional information about this topic.

Using the bit "rfo2" (Figure 12 of the mentioned application note) you could select between the two antennas.

br Travis