ST25R3916B power supply configuration
Hi Community,
I am designing an NFC card reader using a combination of the ST25R3916B NFC frontend and the STM32L476 MCU.
The ST25R3916B has four supply input pins:
- VDD_IO (pin 1): Connected to 3.3V for all serial communication.
- VDD_A (pin 7): Typically connected to 5V by default from the booster.
- VDD_RF (pin 9): Also typically connected to 5V by default from the booster.
- VDD_TX (pin 10): Typically connected to 5V by default from the booster.
In my setup, VDD_IO is powered by a 3.3V supply, while VDD_A, VDD_RF, and VDD_TX are powered by a 5V booster supply, as seen in the ST25R3916B-EMVCO reference schematic.
My question is: Is it okay or recommended to supply these three pins (VDD_A, VDD_RF, and VDD_TX) with 5V? I originally planned to power everything with a single 3.3V supply, but I noticed in the reference schematic that they are supplied with 5V. Would it make any difference if I powered these three pins with 3.3V instead of 5V? Reducing the number of supply voltages by using a 3.3V supply would make the design cheaper and eliminate the need for a booster IC, but would this negatively impact the NFC TX and RX performance?
Regards,
SB