Skip to main content
Hossein Haji
Associate III
September 27, 2023
Solved

ST25R95 WRITE ON SMART CARDS

  • September 27, 2023
  • 2 replies
  • 1293 views

Hello everybody, We hope you are doing well.
we planned to use ST25R95 chip to create a smart card reader that can communicate with all smart cards and java cards (MIFARE and NFC). we read in ST25R95 datasheet that this chip does not support write action in all standards(ISO/IEC). We know we can use PN512 chip that fulfills all needs we have.
Does anyone know PN512 can be replaced by ST25R95?
Can we have full read/write access to all tags MIFARE and NFC mode in all standards(ISO/IEC) by using ST25R95?

Thanks in advance.
Best regards.

This topic has been closed for replies.
Best answer by Brian TIDAL

Hi,

all ST25R readers are able to send Command-APDU and to receive Response-APDU to/from Type 4 tags.

Rgds

BT

2 replies

Brian TIDAL
Technical Moderator
September 28, 2023

Hi,

ST25R95 reader supports

  • NFC-A / ISO14443A tags (T1T, T2T and T4AT tags)
  • NFC-B / ISO14443B tags (T4BT tags)
  • NFC-F / FeliCa™ reader mode (T3T tags)
  • NFC-V / ISO15693 reader mode (T5T tags)
  • ST25TB

MIFARE is a generic brand covering several types of tags. For example, the Mifare UltraLight is a T2T tag that is supported by the ST25R95. I guess you are referring to Mifare Classic. Such tag use proprietary authentication and ciphering. ST25R95 supports the physical framing used for those tags. The support of the proprietary authentication and ciphering on top of ST25R95 cannot be provided by ST for legal reasons (see https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/security-features-in-compatible-with-st25r95-tags/m-p/245273https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/cr95hf-mifarecard-1k-memory-read-write-method/td-p/87096  and others posts related to this topic). I would not recommend to use such old technology cards being now completely broken for more than 12 years.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Hossein Haji
Associate III
October 1, 2023

Thank you so much for your reply.
We have another question, is it possible to send command APDUs to JAVA and DESFire cards and get response APDUs by ST25R95?

Brian TIDAL
Brian TIDALBest answer
Technical Moderator
October 2, 2023

Hi,

all ST25R readers are able to send Command-APDU and to receive Response-APDU to/from Type 4 tags.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.