Skip to main content
Lakshmikanth
Associate II
December 23, 2021
Solved

ST25RU3993-EVAL - access memory bank of temperature sensor

  • December 23, 2021
  • 6 replies
  • 3360 views

Unable to access memory bank of the temperature sensor to get the temperature data.

Hi,

I am working on ST25RU3993-EVAL board for reading the temperature from RFM3200-AFR temperature sensor.

I am finding very difficult in reading the temperature code from temperature Sensor tag memory.

Can anyone help me on how can i access a particular memory location using the SDK source code provided by the ST.

Thanks in advance..

This topic has been closed for replies.
Best answer by Nick K

Hello,

The demo application are generated and tested with VS2017. To open the demo launch ".Applications\STUHFL_demo\STUHFL_demo.sln". This solution has 2 project. The executable demo project STUHFL_demo itself and the STUHFL DLL project. To build use in VS the menu "Build - Rebuild Solution". This first build the stuhfl.lib and dll and then the STUHFL_demo. The STUHFL_demo project reference to the stuhfl.lib file in its linker settings and build only correct when a stuhfl.lib is already generated.

Can you confirm that you are able to read USER memory from the TAGs that are part of the eval kit ?

Are you able to select one of these two TAGs from the kit and read only this, to check that Gen2_Select works for your setup ?

6 replies

Ulysses HERNIOSUS
Technical Moderator
December 23, 2021

Hi LS.7,

I don't know the details of this sensor tag. Where is the sensor data accessible? From user memory?

Any special procedures required?

Any specific place you are struggling?

Best Regards, Ulysses

Lakshmikanth
Associate II
December 23, 2021

Thank you Ulysses for your reply.

I was able to detect the tag in device mode. When the Tag is detected by the EVAL board, I could only access fewer information related to the tag with the help of the structure mentioned below.

typedef struct {

  uint32_t              timestamp;           /**< O Param: Tag detection time stamp. */

  uint8_t               antenna;            /**< O Param: Antenna at which Tag was detected. */

  uint8_t               agc;              /**< O Param: AGC measured when TAG found. */

  uint8_t               rssiLogI;            /**< O Param: I part of Tag logarithmic RSSI. */

  uint8_t               rssiLogQ;            /**< O Param: Q part of Tag logarithmic RSSI. */

  int8_t               rssiLinI;            /**< O Param: I part of Tag linear RSSI. */

  int8_t               rssiLinQ;            /**< O Param: Q part of Tag linear RSSI. */

  uint8_t               pc[STUHFL_D_MAX_PC_LENGTH];   /**< O Param: Tag PC. */

  STUHFL_T_InventoryTagXPC      xpc;              /**< O Param: Tag XPC. */

  STUHFL_T_InventoryTagEPC      epc;              /**< O Param: Tag EPC. */

  STUHFL_T_InventoryTagTID      tid;              /**< O Param: Tag TID. */

} STUHFL_T_InventoryTag;

I want the Temperature code. In the application note AN002F38, it is mentioned as below:

"As with the On-Chip RSSI Code, reading the Temperature Code is a two-step process requiring standard UHF Select and Read commands.

1. Send a standard Class-1 Generation-2 UHF Select command with the parameters described in Table 6 to initialize the temperature sensor and calculate a Temperature Code.

2. Send a standard Class-1 Generation-2 UHF Read command to retrieve the Temperature Code from the tag memory at the location given in Table 7."

0693W00000HpfLAQAZ.pngHow can i send select commands and access the particular memory bank so that i can fetch the temperature code and calculate the actual temperature.

How to read a memory bank using SDK source code provided by the ST.

I want to know if a particular API is available to achieve this and in which place in the source code should i use it.

The application note and the related documents are attached below for your reference.

Lakshmikanth
Associate II
December 23, 2021
Nick K
ST Employee
January 17, 2022

Hello,

thanks for the application note of the sensor TAG. 

according to the application note the sensor TAG needs 3ms continuous wave after the Gen2_Select command before any further command from the reader.

The actual ST25RU3993 do not allow this out of the box. Although, the Gen2_Select command is a separate API calls the FW

collects Gen2_Select commands and send them direct before scanning for TAGs with the Gen2_Query commands.

There is no delay after the Gen2_Select command, as this is not needed under normal conditions.

To add a delay after the Select before the inventory you need to modify the FW first.

The easiest would be to add a HAL_Delay(3); to the functions

static void inventoryGen2(void) in file evalAPI_commands.c

In this function search for "performSelectsGen2();" and add there a delay of 3ms afterwards

With this fix then do the following to select, inventory and read a TAG

To send a Gen2_Select and a following Gen2_Read command please use the following API functions.

NOTE: The Gen2_Select API do not send any command by itself it only store the "select" request(s) in the FW. 

The FW executes then all Gen2_Select commands when running an inventory, as discussed above.

-> This means in your case execute an Gen2_Select, followed by an InventoryRunnerStart and when your TAG is found send a Gen2_Read command.  

For the Gen2_Select and Gen2_Read please use the following API

1. Select:

STUHFL_DLL_API STUHFL_T_RET_CODE CALL_CONV Gen2_Select(STUHFL_T_Gen2_Select *selData);

with 

typedef struct {

  uint8_t               mode;      /**< I Param: Select mode to be applied (CLEAR_LIST, ADD2LIST, CLEAR_AND_ADD). */

  uint8_t               target;     /**< I Param: indicates whether the select modifies a tag's SL flag or its inventoried flag. */

  uint8_t               action;     /**< I Param: Elicit the tag behavior according to Gen2 Select specification. */

  uint8_t               memoryBank;   /**< I Param: Bank (File, EPC, TID, USER) on which apply the select. */

  uint8_t               mask[STUHFL_D_GEN2_MAX_SELECT_MASK_LENGTH];  /**< I Param: Selection mask. */

  uint32_t              maskBitPointer; /**< I Param: Bit starting address to which mask is applied (bit address). */

  uint8_t               maskBitLength; /**< I Param: Mask length in bits. */

  uint8_t               truncation;   /**< I Param: Truncate enabling. Not supported yet, must be set to zero */

} STUHFL_T_Gen2_Select;

The parameter target, action, memoryBank, mask, truncation are as defined in the UIHF Gen2 standard.

Accodring to the application note, in case of temperature measurement with this sensor TAG you could use the default initalization values, except the memoryBank.

eg:

STUHFL_T_Gen2_Select Gen2Select = STUHFL_O_GEN2_SELECT_INIT(); // Set to FW default values

Gen2Select.memoryBank = STUHFL_D_GEN2_MEMORY_BANK_USER; // set memory bank

// mask and maskBitLength is empty by default   

// Execute the Gen2_Select command

Gen2_Select(&Gen2Select);

2. Run inventory

or execute the following API to run just one inventory round

STUHFL_DLL_API STUHFL_T_RET_CODE CALL_CONV Gen2_Inventory(STUHFL_T_InventoryOption *invOption, STUHFL_T_InventoryData *invData);

3. Read

For the final Gen2_Read please use the following API

STUHFL_DLL_API STUHFL_T_RET_CODE CALL_CONV Gen2_Read(STUHFL_T_Gen2_Read *readData);

with

typedef struct {

  uint32_t              wordPtr;          /**< I Param: Word address to which read data. */

  uint8_t               memoryBank;         /**< I Param: Bank (File, EPC, TID, USER) to which read data. */

  uint8_t               numBytesToRead;       /**< I Param: Number of bytes to read. */

  uint8_t               pwd[STUHFL_D_PASSWORD_LEN]; /**< I Param: Password. */

  uint8_t               numReadBytes;        /**< O Param: Number of effectively read bytes. */

  uint8_t               data[STUHFL_D_MAX_READ_DATA_LEN];  /**< O Param: Read data. */

} STUHFL_T_Read;

In your case the memoryBank must be set to STUHFL_D_GEN2_MEMORY_BANK_RESERVED and the wordPtr must be set to WordAddr 0x0E

BR Nick

Lakshmikanth
Associate II
January 31, 2022

Hi Nick. Thank you so much for your efforts.

  

As mentioned by you, I made the changes and called the select api, followed by inventory and read.

But still not getting the temperature data. I am getting only zeroes.

However, I noticed the following:

1. When STUHFL_T_Gen2_Select variable is declared, initialized and Gen2_Select() function is called, Only the first 'if' block inside it is getting executed, as all the parameters are set to default except memory bank.

2. Inside performSelectsGen2() function, the gen2Select() function is not getting called as numSelects value is 0.

/****************************************************************************************************** 

static void performSelectsGen2(void)

{

 for(uint32_t i=0 ; i<numSelects ; i++) {

   gen2Select(&selParams[i]);

 }

 StoreTestData(TEST_ID_GEN2_SELECT_T4MIN, sizeof(uint16_t), (uint8_t*)&gen2Configuration.T4Min);

}

 /*****************************************************************************************************/

 And moreover selParams will be sent as the argument for gen2Select, which are all zeroes.

I have added the HAL_Delay(3), right below the PerformSelectsGen2() inside inventoryGen2() in evalAPI_commands.c file. That particular part of code is attached below for reference.

/*****************************************************************************************************/

    //

   // Search for TAGs ..

 //   

performSelectsGen2();

HAL_Delay(3);

tagCnt = gen2SearchForTags(autoAckMode, &p);

 // update counters

 increaseRoundCounter();

 /****************************************************************************************************/

The While loop inside my main function looks like this.

 /****************************************************************************************************/

while(1)

{

  STUHFL_T_InventoryOption invOption;

  STUHFL_T_InventoryData invData = STUHFL_O_INVENTORY_DATA_INIT();

  // apply data storage location, where the found TAGs shall be stored

  STUHFL_T_InventoryTag tagData[STUHFL_DEVICE_MODE_MAX_TAGS] = { 0 };

  invData.tagList = tagData;

  // setup options

  invOption.rssiMode = STUHFL_D_RSSI_MODE_2NDBYTE;

  invOption.roundCnt = 1;

  invOption.inventoryDelay = 0;

  invOption.options = 0x00;

  // assign correct size of applied tag storage

  invData.tagListSizeMax = STUHFL_DEVICE_MODE_MAX_TAGS;

  //doInventoryCfg(true, false, STUHFL_D_ANTENNA_1); // single TAG

  doInventoryCfg(false, true, STUHFL_D_ANTENNA_2); // multiple TAGs

  // Single round inventory with tags post process

  Gen2_Inventory(&invOption, &invData);

  LOG("Found tags: %d\n",invData.tagListSize);

  // Multiple rounds inventory with tags on the run processing

  inventoryCycleCbCnt = 0;

  Inventory_RunnerStart(&invOption, cbInventoryCycle, NULL, &invData);

  /**

   * NOTE: Starting the inventory runner is a blocking call. Whenever

   * transponders found the STUHFL_T_InventoryCycle callback is called.

   * Within this callback processing of the data should take place.

   *

   * To stop the runner and return from the Inventory_RunnerStart function

   * there are 2 possibilities.

   *

   * 1. A call to Inventory_RunnerStop. Can be called from the callback

   * 2. When the number of requested rounds are executed

   *

  */

  for(int i = 1; i < 16; i++) {

   invOption.roundCnt = i;

   inventoryCycleCbCnt = 0;

   

   

  /*1.Configure and call select command*/

   STUHFL_T_Gen2_Select Gen2Select = STUHFL_O_GEN2_SELECT_INIT();

   Gen2Select.memoryBank = STUHFL_D_GEN2_MEMORY_BANK_USER;

 // Gen2Select.maskBitPointer = 0xE0;

   Gen2_Select(&Gen2Select);

 /*2.start the inventory round*/

Gen2_Inventory(&invOption, &invData);

 /*3.Read the TAG*/

STUHFL_T_Gen2_Read readData;

readData.memoryBank = STUHFL_D_GEN2_MEMORY_BANK_RESERVED;

readData.wordPtr = 0x0E;

readData.numBytesToRead = 8;

Gen2_Read(&readData);

}

}

/****************************************************************************************************/

Please tell me if I am doing something wrong.

Ulysses HERNIOSUS
Technical Moderator
January 31, 2022

Hi,

browsing through I think there may have been one line missing:

Gen2Select.mode = STUHFL_D_GEN2_SELECT_MODE_CLEAR_AND_ADD;

as the default seems to be STUHFL_D_GEN2_SELECT_MODE_CLEAR_LIST.

BR, Ulysses

Lakshmikanth
Associate II
January 31, 2022

Ok. Thank you for your quick response.

I will check and update

Nick K
ST Employee
February 2, 2022

Hello Lakshmikanth,

User Ulysses is right, the default Gen2Select.mode is STUHFL_D_GEN2_SELECT_MODE_CLEAR_LIST which only clears the internal lists of select commands that 

shall be executed before the gen2SearchForTags. The correct Gen2Select.mode is STUHFL_D_GEN2_SELECT_MODE_CLEAR_AND_ADD

Have you tried with some other "standard" Gen2 TAG (use the one that is part of the ST25RU3993 EVAL/HPEV package) to select it and for example read the User memory ?

In the SDK package you find C demo code example to inventory, read and write user memory for 1 selected TAG.

This code is in function "void demo_evalAPI_Gen2RdWr()" in file "STUHFL_demoEvalAPI.c" of the solution ".\Applications\STUHFL_demo\STUHFL_demo.sln"

BR

Lakshmikanth
Associate II
February 4, 2022

Hello Nick,

As you told, I tried to read the Tag using the C demo code in the SDK package.

I was not able to read the tag data.

It says the Tag cannot be read. I tried with 2 temperature tags RFM3200 and 2 moisture tags RFM2100.

But I couldn't read the data from any tag.

the output which i got is pasted below.

*******************************************OUTPUT******************************************

Choose an action below:

    v: Version from HOST side

    T: Toggle tuning mechanism

    t: Tune frequencies

    g: Gen2Inventory from HOST side

    i: InventoryRunner from HOST side (1000 rounds)

    I: InventoryRunner from HOST side (infinite loop)

    r: Read/Write tag from HOST side

    G: Gen2 Generic Command from HOST side

    q: quit

r

Reading/Writing data on tag

Tuning Profile frequencies: algo: STUHFL_D_TUNING_ALGO_SLOW

--- Gen2_Inventory Option ---

rssiMode  : 6

reportMode : 0

--- Round Info ---

tuningStatus: TUNED

roundCnt  : 1

sensitivity : 3

Q      : 1

adc     : 0

frequency  : 866900

tagCnt   : 1

empty Slots : 14

collisions : 0

preampleErr : 0

crcErr   : 0

--- 001 ---

agc     : 15

rssiLogI  : 12

rssiLogQ  : 14

rssiLinI  : 38

rssiLinQ  : 127

pc     : 30 00

epcLen   : 12

epc     : 00 00 00 00 00 00 00 00 00 00 83 50

tidLen   : 0

tid     :

--- Selecting TAG ---

00 00 00 00 00 00 00 00 00 00 83 50

Tag cannot be read

--- Write 1st word TAG data ---

    => 0xa55a

Tag cannot be read

--- Write 1st word TAG data ---

    => 0xcccc

Tag cannot be read

Task finished .. press a key to continue

************************************************************************************

Lakshmikanth
Associate II
February 24, 2022

Can someone help me in reading the tag data

Nick K
Nick KBest answer
ST Employee
February 4, 2022

Hello,

The demo application are generated and tested with VS2017. To open the demo launch ".Applications\STUHFL_demo\STUHFL_demo.sln". This solution has 2 project. The executable demo project STUHFL_demo itself and the STUHFL DLL project. To build use in VS the menu "Build - Rebuild Solution". This first build the stuhfl.lib and dll and then the STUHFL_demo. The STUHFL_demo project reference to the stuhfl.lib file in its linker settings and build only correct when a stuhfl.lib is already generated.

Can you confirm that you are able to read USER memory from the TAGs that are part of the eval kit ?

Are you able to select one of these two TAGs from the kit and read only this, to check that Gen2_Select works for your setup ?