ST25RU3993 higher than expected power on RX
- February 24, 2023
- 3 replies
- 1608 views
Hello,
I'm currently prototyping a custom design utilizing the ST25RU3993 which should be nearly identical to the reference design HPEV. I've removed the external PA and 2nd antenna, but otherwise the design is very similar. I've attached the schematic for comparison. Where available, I've followed the reference layout as closely as possible.
The board is showing poor read rates (low distance, ~50% success rate for consistent tag-antenna positions) which I suspect is the result of the following: the RX probe point (equivalently RF-TP4 on the eval kit) shows almost 5dBm at the carrier frequency when measured with the spectrum analyzer. I understand this should be closer to -14dBm.
Am I missing something obvious from my design? Or could this be a possible result of an assembly issue? Looking forwards to any insight into the issue or further testing I can perform.
Thanks!