Skip to main content
YChav.3
Associate
September 13, 2022
Solved

ST25RU3993-HPEV read tags in 3ft only

  • September 13, 2022
  • 1 reply
  • 610 views

At ST25RU3993-HPEV firmware how to control an antenna distance? For eg. I want an antenna to read tags in 3ft only.

This topic has been closed for replies.
Best answer by Nick K

Hello YChav.3

In general the read range can be limited with the TX power settings. The less Tx power the less read range. A strong dependency is also given through the used antenna. Also the used Tag and frequency can have a impact on the read range. This means one Tx power settings can limit the read range for one setup, but could allow to read further with a different setup.

BR

Nick

1 reply

Nick K
Nick KBest answer
ST Employee
October 14, 2022

Hello YChav.3

In general the read range can be limited with the TX power settings. The less Tx power the less read range. A strong dependency is also given through the used antenna. Also the used Tag and frequency can have a impact on the read range. This means one Tx power settings can limit the read range for one setup, but could allow to read further with a different setup.

BR

Nick