Skip to main content
spp.1
Visitor II
June 2, 2022
Solved

ST25RU3993HPEV - suddenly not detecting tag

  • June 2, 2022
  • 1 reply
  • 655 views

I have been using the ST25RU3993HPEV board for the Tag detection. Earlier the board is performing well and it was detecting tag. But suddenly reader is not detecting tag.

Is there any chance for power amplifier regulator has gone bad?

If the tag is kept on the surface of the antenna, it will be detected at some point.

This topic has been closed for replies.
Best answer by Bart Herse

Dear SPP.1

is the supply voltage for the power amplifier still present? --> check voltage between pin 1 and 2 on J21. Note to switch on the RF before doing the this measurement.

Is the HPEV reader still able to detect tags, when switching to the internal power amplifier?

Cheers,

B

1 reply

Bart Herse
Bart HerseBest answer
Technical Moderator
September 27, 2022

Dear SPP.1

is the supply voltage for the power amplifier still present? --> check voltage between pin 1 and 2 on J21. Note to switch on the RF before doing the this measurement.

Is the HPEV reader still able to detect tags, when switching to the internal power amplifier?

Cheers,

B