Skip to main content
Mickaël Bucher
Associate III
January 27, 2022
Solved

STM32CubeExpansion_NFC4 set RF password with I2C

  • January 27, 2022
  • 1 reply
  • 681 views

Hi,

I use a ST25DV04K with STM32CubeExpansion_NFC4_V2.0.2.

 is it possible to set a RF password with an I2C function ?

if yes, Could you give me some examples ?

Best regards

Mickaël

This topic has been closed for replies.
Best answer by JL. Lebon

Hello Mickaël,

It is not possible to write or read RF passwords from the I2C interface.

It is also not possible to write or read I2C password from RF interface.

The passwords and security sessions for RF and I2C are completely independent and isolated for security reasons.

Best regards.

1 reply

JL. Lebon
JL. LebonBest answer
ST Employee
January 28, 2022

Hello Mickaël,

It is not possible to write or read RF passwords from the I2C interface.

It is also not possible to write or read I2C password from RF interface.

The passwords and security sessions for RF and I2C are completely independent and isolated for security reasons.

Best regards.