Skip to main content
fredj0207
Associate II
December 6, 2023
Solved

Support for ICODE ILT tags

  • December 6, 2023
  • 1 reply
  • 1304 views

Hi,

I would like to use NXP ICODE ILT tags (ISO18000-3) with the ST25R3911B device.

As ISO18000-3 is similar to ISO15693, is it possible to use stream mode (as in RFAL) to support ISO18000-3 ? Is there any HW limitation ?  If no, did any of you already do this ?

Regards

Fred

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi Fred,

 

thx for this information. Yes it should be possible to support the ILT-M by using stream mode. However I am not aware of any actual implementation where you could start off from. 

Did you start this? Any insights already? In case you are running into detailed problems, please let me know and I can try to support.

BR, Ulysses

1 reply

Ulysses HERNIOSUS
Technical Moderator
December 7, 2023

Hi Fred,

 

ISO18000-3 defines three different operating modes. ICODE ILT is using Mode3. Using stream mode it should be possible to support Mode3 and also these tags but I am not aware of any reference implementations where you could start off.

Mode1 is equivalent to ISO15693 and as such supported. Mode 2 to my knowledge might only be supported in transparent mode.

Looking around on distributors I find the ILT marked as "Not for new Designs" or "Last Time Buy". How come you want to support those?

BR, Ulysses

 

 

fredj0207
fredj0207Author
Associate II
December 7, 2023

Hi Ulysses,

It will be ICODE ILT-M (available in mass production) using ISO18000-3M3 and EPC for fast anticollision.

Regards,

Fred

 

Ulysses HERNIOSUS
Technical Moderator
February 1, 2024

Hi Fred,

 

thx for this information. Yes it should be possible to support the ILT-M by using stream mode. However I am not aware of any actual implementation where you could start off from. 

Did you start this? Any insights already? In case you are running into detailed problems, please let me know and I can try to support.

BR, Ulysses